XMC™ Forum Discussions
Hello,
I use a XMC130T038 and I implement an I2C. When I'm in debug mode, my system starts but is blocked directly in I2C init.
I have the save problem in release mode. I can bypass by cut the power and then put the power on. But when i use NVIC_SystemReset the system is blocked again. does someone know where the problem come from ?
Already thank you.
Show LessHello all
I have a question about using OneEye (or any GUI builder)
I want to interface with an xmc4700 by attaching an arduino screen to the female headers I've soldered on an XMC4700. The plan is to read sensor data from the xmc and display it on a screen. This obviously implies writing code to read sensor data, then display it on a screen.
I looked around and infineon provides a few GUI builders such as SeggerAppWizard, OneEye and emWin. Are these the things to use for this task? I was thinking of using the arduino IDE too with the xmc library, is this possible?
Many thanks 🙂
Show Less
Hi,
I confess that I was very disappointed with the poor analogue integration of the XMC7000. ADC with only 1MSPS and no analogue comparators. Many cortex-M0's nowadays have much better analogue integration than that. In addition to not having high resolution PWM.
I hope that Infineon is planning to release new items in this family with better analogue integration and without so much flash memory and CAN-FD ports to lower the price. Making this family competitive in high-end power conversion applications.
Dears
I would like to port application which was developed on KIT_XMC14_BOOT_001 using XMC1404-Q064x0200 to XMC1302-T038x0200.
I tried to create custom BSP, follow all available documentation for Modus Toolbox.
But I have the following problem:
Could you help me?
Regards
Pietro
Hi guys,
I just started using XMC4500 Relax Lite and wanted to understand how I can use the CCU4 as a timer. I need to count a certain number of <X> ms and do an action when the timer expires. It would be great if someone shares the method to do so or reference material on how to do it !!!
Thanks in advance
Show LessDears.
There are four slave devices in SPI MASTER. Why can only set the number of slave to 3 in APP, while the maximum display can be set to 8?Thanks.
Show Less
Dear Infineon Team
We are very new to XMC based MCUs and are really confused in following things
We have selected the part XMC1403Q040X0200AAXUMA1 (VQFN-40) for one of our legacy products
1. Reset pin: No reset pins are provided in the Pin description section. Currently we chose P0.3 as reset pin, Please let us know the choice is appropriate.
2. External Oscillator(48MHz) is used and connected to P0.10 pin, is it the right pin?
3. Which pins could be used to program/debug the IC?
4. Which are the PWM output pins that we can use independently?
Please help me to sort these things as I am not getting any articles related to the same.
Show LessGreetings of the day,
Currently am working on 'Over Current Protection' in BLDC Hall sensor Controlling using XMC1300 MCU with custom motor designed for max current = 150A and trying to set over current limit, but here am bit confused with below 2 parameters MOTOR0_BLDC_SCALAR_OVER_CURRENT and MOTOR0_BLDC_SCALAR_SHORTCIRCUIT_CURRENT ? can you explain me in detail how to configure above 2 parameters and how it works ?
1) Am configuring MOTOR0_BLDC_SCALAR_OVER_CURRENT to 5A and motor stops initially in Power ON, It is detecting fault and entering into Protection ISR ? Is it considering the difference between bound0 and bound1 ?
2) In UM of XMC1300 It is mentioned that Event is trigger when it is in boundary limits, but in SW it is mentioned that after exceeding boundary limits only over current is detected. which is to be considered ?
Note: Please check the below 2 Images Highlighted.
3) I have go through the BLDC_SCALAR_HALL_XMC1300 user guide, but am unable to detect fault,
below is the DC bus voltage (Blue)and DC bus current (Yellow) captured at 1000 RPM and getting noise at DC input (DC current). Any issue with noise I have tried using averaging method also but it is not detecting fault when set to 5A.
Can you please help me to come out of these issue
Thanking you
Suraj, N
Show LessHi all,
On a XMC1402 I toggle in software one GPIO (P2.10) but I need to be sure the pin state is low if I halt the CPU or in case of a breakpoint event.
I can't link the pin to a peripheral because CCU8 is already fully used.
Is there a way to set the passive level state for a GPIO?
Can a function be called just after every breakpoint to set the system to a known and safe condition?
Thanks and best regard.
Show LessHello,
I need to know if XMC7000 supports the SENT protocol communication?
Thank you in advance.