Announcements

Help us improve the Power & Sensing Selection Guide. Share feedback

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

XMC™ Forum Discussions

Tarun_M
XMC™
Hi,I have a doubt regarding the ADC in XMC4400. I have connected the ADC input pin P15.8 to the 3.3V pin of the XMC4400 board. The ADC is configured t... Show More
Kawata
XMC™

I would like to receive DMX512 signals for lighting control.
Is there any sample code for DMX512 with XMC?

Regards,
Kawata

RajivB
XMC™
Dear Infineon, Any example to read 32-bit I2S PCM data using XMC4500 using DMA, which is the standard way it is handled in other MCUs like Microchip, ... Show More
Horizonxx
XMC™
Hello,Actually I am trying to read time interval  for a function to run using following code, expected time to run is in nano seconds.Q1 - Can I read ... Show More
User12255
XMC™
I am design a new application where XMC4800 is used as EtherCAT slave with PMSM FOC. I started with EtherCAT slave stack demo for XMC4800 and I added ... Show More
Tarun_M
XMC™
Hi,I am interfacing the ADC of XMC4400 to read an analog value and display the corresponding digital value on a 16x2 LCD. The ADC pin I have connected... Show More
Translation_Bot
XMC™
Please advise: I added the PMSM_FOC module to the ETHCAT_SSC_AUT_BASE_XMC48, sample code. In configuring the ADC it was found that Acquisition B could... Show More
eidetech
XMC™
Hi I have downloaded the XMC flasher tool, and when I opened it and tried to connect for the first time I was prompted that there was a new version of... Show More
tsd
XMC™
请教,我目前正在使用的是,XMC4800_E196K2048的芯片,工程是ETHCAT_SSC_AUT_BASE_XMC48,我在这个工程上添加了,PMSM_FOC的模块,但U,V,W三相引脚,无法配置P0_0,P0_1,P0_2,P0_3,P0_4,P0_5,这六个引脚。但我明明没有使用这个六引脚... Show More
wsnfly
XMC™
My purpose is to control the private server motor. Because most servo motors are controlled using pulses. So if it involves the acceleration and decel... Show More