Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

XMC™ Forum Discussions

XMC™ Forum Discussions

Sort by:
Markus_S
XMC™
Hello!Can a crystal be connected to an XMC1100Q024? And if yes, where? Is there a hardware manual available for those devices?Many thanks! Show More
Anonymous
XMC™
Hi,,,,am new to SP37. Can you give any ideas??
Travis
XMC™
Our previous TIP mentioned about peripherals triggering the DMA for data transfer from a source to a destination with a DLR.However we can also have p... Show More
User18952
XMC™
hello,I have the following Hexagon XMC4200 Kit. How can i utilize the SPI on that kit?I mean i can not use the interface pins of the spi as they are n... Show More
User16529
XMC™
Hi!I'd like to run the OPC UA example provided by Infineon on the XMC4300 relax kit and I'd like to communicate through the seral port instead of the ... Show More
User18908
XMC™
HelloThe trouble is that on the board KIT_XMC48_RELAX_ECAT_V1 it is impossible to activate any CAN nodes, except Node 1, for which a transceiver is pr... Show More
User18926
XMC™
We are using multiple IN EPs in our design. I configure the endpoints in the USB_Descriptor_Configuration_t configuration_descriptor in Dave/Generated... Show More
User8734
XMC™
Hello everyone,I have a simple task -> transmit data uint16_t srcBuffer[1024] -> UART at 1Mbod speed.I took example "DMA003_USIC" from this thread MEMORY->UART... Show More
User18369
XMC™
Hello,I´m trying to receive an extern interrupt.I used Dave APPs(- EventDedector ; EventGenerator; NVIC; DIGITAL IO)I never get into the service routi... Show More
User18744
XMC™
Using the PWM app in Dave, I see that the compare value is dependent on the Frequency and the the duty cycle.
How is this calculated?