Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

XMC™ Forum Discussions

XMC™ Forum Discussions

Sort by:
rst
XMC™
I need a fast real-time data stream from device (USB-device) to PC (USB-host). I use a large isochronous endpoint (packet length <= 1023 bytes).The da... Show More
User18369
XMC™
Hello,I´m not able to select Pins in the XMC 4300 EtherCat example:If i try to select Pin Number (Port) it ends in - Solver time out hast occured....... Show More
User16843
XMC™
Hi all: I am facing the old problem of SPI APP(4.3.28) in receiving data from a ADC. The SPI app operate in full duplex mode, I used the SPI APP (... Show More
User16575
XMC™
Hi,Im using the UART App in DAVE to receive bytes asynchronously. I dont know how many bytes I will receive ahead of time, but I do know that they wil... Show More
User14248
XMC™
Hello,I have a problem when enable WFE while enable UART receive interrupt.For WFE, I set the function to XMC_SCU_CLOCK_SetSleepConfig(XMC_SCU_CLOCK_S... Show More
User16529
XMC™
Hi!I'm testing the opc ua server example OPCUASERVER_LWIP_XMC47 on my xmc4800 automation board, but the server doesn't start. In the function opcua_in... Show More
User17850
XMC™
Hi all,
I'm new on Infineon, I've a XMC1202x016 it's possible to flash/debug it with the ulink2 programmer via SWD programming?
Thanks.
User18369
XMC™
Hello,I´m working with an XMC4300. Sometimes I have the problem that the uC end in a Hard Fault.I have no clue what to do. I enabled Hard Fault debugg... Show More
User14248
XMC™
Hello,I am working on the XMC4800 and implementing a receive interrupt. Somehow the interrupt is not working but the data can be readout using functio... Show More
User19102
XMC™
Hello everybody,I have been working with XMC4400 by using both DAVE and Keil uVision . When I try to migrate projects from Dave to uVision I can make ... Show More