Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

XMC™ Forum Discussions

Sort by:
xiphi
XMC™

我司使用的是xmc4000系列和xmc1000系列,我目前负责XMC1404芯片,我想请问新手应该如何入门,怎么操作芯片引脚的寄存器,如何设置推挽输出之类的。

gachetp
XMC™
Hello, I use an XMC45 I would like to use the ASCbootloader for that, I connected the UART pin to (1.4 et 1.5) like it's ask, I put my soft in ASC mod... Show More
Maddin
XMC™
Hi guys, I am in the process of creating a new environment for an Incurcit programming application. For this I have to flash a "XMC1302-0064" with an ... Show More
amanning
XMC™
A XMC program can be set to run in either the cached or non-cached Flash memory space. Our application runs in the cached address space which allows i... Show More
ericjoy
XMC™
Hi,  I have use STM32F4 years ago, and migrate to XMC4800 recently for BLDC drive and ethercat communication. Everybody knows that microprocessor are ... Show More
AndreDomps
XMC™
Hello I am a physics teacher and I intend to examplifies the principle of radars using the Sense2GoL development kit,as explained here : https://www.infineon.com/cms/en/product/promopages/makeradar/plug-and-play/... Show More
nkotak
XMC™
Hello there, We are working on bring-up of our custom board based on XMC4400 and wanted to know if we can program our custom boards using XMC4400Platf... Show More
User9266
XMC™
Dear All 目前我仍在DAVE3.1.10上進行開發, 需要使用到IEC 60335 Class B Library 已向供應商取得Class B Library與說明手冊, 但供應商無相關的經驗可以支援 目前先依照內附的手冊建立含Class B的專案進行測試, 但實際試做時說明文件與檔案有些... Show More
jsmith678x
XMC™

Hi,

Which is the best way to modify the prebuilt CM0P image? Also how to include it in my project?

 

Bellawu
XMC™

来自一位客户的咨询:

我司采用的是英飞凌xmc系列芯片,请问您有1400系列的例程吗?以前的技术论坛的资料都没了。