XMC™ Forum Discussions
Hi
I can trap CCU8 from external event with external pin to generate the event 2.
However I would like to trap / untrap with internal function call as well.
Would you please give me some example project.
Thanks in advance
Show LessHello Infineon,
My team is doing a feasibility study on using the XMC7200 microcontroller for our project. One of the requirement is to have parallel communication between the XMC7200 with external RAM.
My question is that is there an already written XMC7200 Hyperbus driver support for external RAM (parallel memory interface)?
Show LessHello,
what's the relationship between "time interval" in APP configuration and "TIMER_SetTimeInterval" in function?
You can see I have set the "Time interval[usec]" to 1200, and then I use function "TIMER_SetTimeInterval" set to 1.
Then what is the real time interval I have set? After How long time will the "time interval event" be triggered?
Thanks!
Show Less
Dear supporter
I want to translate the following KBA, please confirm to my work.
Best Regards.
Show LessDear MTB Team,
There is no suitable template project for XMC7200D-F176Kxxx that can be used as a starting point for development.
We need a single core and a multi core empty application that is suitable for the XMC7200D-F176K as a starting point. The existing multi core empty application is buggy and can not be used.
Best Regards,
Mubeen Haadi.
Show LessHello,
I am using XMC4800 for my project. I want to implement a software interrupt. Can I use an unassigned interrupt node for the software interrupt (e.g. node 9)? Is there a chance that the interrupt is triggered by the hardware?
thank you!
Show Less
您好,
我使用的xmc4200的开发板,ide是mtb,我想用adc采集三个通道的数据,使用dma的方式搬运数据,三个通道数据转换完成并产生dma中断,这个程序我该怎么写呢?
此致敬意
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/XMC/%E5%A6%82%E4%BD%95%E5%9C%A8%E5%88%AB%E7%9A%84IDE%E4%B8%AD%E4%BF%AE%E6%94%B9%E5%92%8C%E4%BD%BF%E7%94%A8DAVEAPP%E7%94%9F%E6%88%90%E7%9A%84%E5%A4%96%E8%AE%BE%E9%85%8D%E7%BD%AE%E4%BB%A3%E7%A0%81/td-p/500477
Show LessHello,
In our company we use many cards with an Infineon processor, XMC4500.
When we communicate with them in TCP communication
we encounter the same problem that repeats itself on all cards.
General description of the system:
Each system has several cards with an XMC4500 processor,
Once a second we send a command (via TCP) to all cards and wait for a reply.
The system is supposed to be ON 24/7, what happens today is that after a few days (2, 3 days on average) the communication with the card stops and only a reset to the card restores it to activity.
When the communication stops - what happens is that you can't send requests to the specific port, but when you send a ping request it works.
The processor continues to run, the TCP communication stops.
The ETH_LWIP app is set up the same as in your examples.
Do you have any idea what causes this problem and how to solve it?
this is very important to us.
Thank you
Yehudit
Show LessHi, I am working on phase shifted PWMs in XMC4400. By reading the app note below, I have a doubt on PWM generation for PSFB. In Figure 25, two phase shifted pwms are generated. However, in Figure 26, four pwms (two complementary pair) are needed. How do you get the complementary pair (Q21, Q22) for the slave CC81?
Do you have any other ways to generate 120-degree phase-shifted pwms, 6 pwms in total (3 complementary pairs) for 3 half bridges?
Thanks.
Show Less