XMC™ Forum Discussions
Hi Team,
We are working on our own design need help.
We have to Run new motor with the "BLDC_SCALAR_HALL_XMC13_Power_Tool code" using XMC1300 Kit. Changes should be done in the existing code so please help me to continue our testing.
We need required changes in software when we change motor and Shunt resistor(Please see the below link about current sense Amplifier).
What are the changes have to be done in the "BLDC_SCALAR_HALL_XMC13_Power_Tool code" to run Golden motor. More details available in the link below (at last query of the thread dated: Mar 01, 2022 10:44 PM).
" https://community.infineon.com/t5/XMC/Running-BLDC-Motor-continuously-in-Current-Control-Scheme/m-p/337232#M10254 "
Any help would be very thankful.
I am using a xmc relax lite with xmc4700 cpu. The problem is with the debugger. No matter what program I write, it will build just fine. When I go to debug, I get the error message 'Launching Hello Debug' has encountered a problem. I have checked all the windows under the debug drop down, and everything seems fine. I have checked all the possible online fixes, and they don't work.
If you can't get past this error, you can't use the device. I have been stuck for days.... Does anyone have an idea?
Show LessI just started working on Dave and its quite new to me. I created a Dave CE project and was able to get the blink code up and running. I want to add CMSIS DSP library to my project and use the DSP functions in the library.
My barebones Dave CE project already comes with a couple of CMSIS includes. However, I do not see the entire CMSIS includes. I need to also have CMSIS DSP included in the include paths and the library files I think. Can someone guide me on how to get that done?
Thanks
Show LessI am using Dave. I am working with a xmc45 Relax Lite kit. The problem is with the debugger. I can write a simple program like "Hello" and build it. The build works fine. Now, you want to run the debugger. As soon as it is clicked, an error message appears and at that point, you are stuck.
I was seeking help from this forum and was told to click "Yes" on firmware updater. So, here is the problem, where do you fine this firmware updater? I have clicked every icon on the DAVE CE form at least 20 times. The firmware updater fails to appear.
Does anyone have any information on solving this problem?
Show Less
Hi,
I am using xmc7200, serial configuration and writing do not know where to write wrong, can not enter the interrupt can not receive data.
Best regards
Show Less
Hi,
I am planning to use an external reset IC to reset the XMC4800 for power supply design reasons.
The operating voltage range of the XMC4800 is narrow (especially between Min.3.13V and Typ.3.3V), so when considering the voltage detection accuracy and hysteresis of the reset IC, I could not find an IC that can be used at 3.3V VDDP.
Could you please teach me a recommended/available reset IC?
--
Shimamura
Dear Team,
Plz help to solve below points.
1. miniWiggler V3 not being detected in my Windows 11 64bit & x64 based operating system automatically. so is there any place from where I can download its driver to my system.
2. Document for connecting any XMC MCU to miniWiggler V3 connection to be made for programming and debugging.
Thanks in advance for your support.
Show LessHello,
I am wondering wheter it is possible to upload new firmware to XMC4000 microcontrollers by its USB or UART channel. If so, Could anyone guide me on how to do it?
I do not need to debug any code, just upload new firmware.
Thanks in advance.
Show LessHello,
I want to use a XMC4200 as an on-board debugger of a XMC4500. In this way, I could use a USB to upload and debug firmware to the XMC4500.
Is there any place where I can found the firmware that I have to upload to the XMC4200 to work as a on-board debugger. I would like to use a Segger J-link debug.
Is there anyone that help me or give mo some idea on how to do an on-board debugger for mi target XMC4500?
Thanks in-advance.
Show Less