XMC™ Forum Discussions
请问用DAVE打开一个已有的工程,为什么打开总是一片空白?附件图片是打开一个目录下面已有的工程步骤,用import导入最后也是一片空白
我现在用的是XMC4700F100K1536做异步感应电机的FOC控制,有没有DAVE APP生成FOC电机控制相关的DEMO可以参考?单片机可以是相近的,电机可以是PMSM FOC都可以,谢谢
The free-of-charge µC/Probe XMC is has the same functionality µC Probe working with XMC microcontrollers exclusively. It allows easily designing a graphical dashboard with a wide range of widgets to control or fine-tune your XMC application and it includes an 8 channel digital oscilloscope to visualize real-time date, controlled by a dedicated target code that runs on the XMC target.
µC/Probe XMC is simple to install on Windows PC and can be easily connected via the J-Link on board debugger integrated on most of the XMC kits.
Interested? Then register and download to get your µC/Probe XMC instantly.
A quick start tutorial helps to get started in a short time. Show Less
Hello,
i'm missing some UI elements in ModusToolbox DeviceConfigurator (XMC4500) when using SPI with multiple slave select lines.
In my assumption, there have to be multiple SELO0..x lines in pin config when increasing "Number of Slave Select Lines Used", but it is still only one SELO-line configurable.
Ending up in a code generator alert of connected hidden pins. It's totally clear why, but the UI limitation is a little bit frustrating.
It is a bug or a feature?
Thanks in advance,
Thomas
Show LessDAVE FOC APP生成了三对互补的PWM,要是再增加一对互补的PWM,也是CCU8的,该如何设置或者是添加APP呢
I am trying to use the DAC of the XMC4200 together with the DMA, but the data is not being transferred by the DMA controller.
The DAC channel 0 is configured in Data Mode with internal trigger and a frequency of 24kHz. The Service Request, Run and Analog Enable bits are set.
The DMA Line Router (DLR) is configured with line 1 with RS1 = 5, which is DAC.SR0. Line 1 is enabled with LN1 set.
The DMA channel 1 is configured with the Destination Address Register set to 0x48018014, which is the DAC input register. The CFGH.DEST_PER is set to 1 to use DLR line 1 and CFGL.HS_SEL_DST is set to 0 to select Hardware handshaking.
The DMA is enabled with DMACFGREG.DMA_EN set.
As far as I know everthing is configured correctly, but it does not work!
The application is a modified version that used the DMA to send the data to a USIC and that works correctly.
Does anyone have any ideas where the problem could be?
Show LessWhen I power off the microcontroller and then power it on again, the program automatically starts. How can I prevent this behavior? I only want the code to execute when I debug it from DAVE.
Show LessDear supporter
I want to translate the following KBA, please confirm to my work.
Best Regards.
Show LessDear MTB Team,
There is no suitable template project for XMC7200D-F176Kxxx that can be used as a starting point for development.
We need a single core and a multi core empty application that is suitable for the XMC7200D-F176K as a starting point. The existing multi core empty application is buggy and can not be used.
Best Regards,
Mubeen Haadi.
Show Less