XMC™ Forum Discussions
Hi folks,
I am working with XMC4400 plat2go dev board on the CAN communications. Right now, specifically I am trying to implement the usecase of receiving a remote frame from external, and repsonse with a cooresponding data frame as requested.
From the MultiCAN application Note https://www.infineon.com/dgdl/Infineon-MultiCAN-XMC4000-AP32300-AN-v01_00-EN.pdf?fileId=5546d4624e765da5014ed91d6be32110, in section 2.3.3 Software control of message transfer, what I read is the TX message object can do remote frames' reception and reponsing automatically as long as having a matching id with the remote frame: (quote below)
"Table 2 lists the maximum number of m essage objects in XMC4000 derivatives and the message objects
which can be set up for transmit or receive operation according to the selected value for control bit DIR.
TX message object (DIR=1); Set for data frames’ transmission and for remote frames’ reception.
RX message object (DIR=0); Set for data frames’ reception and for remote frames’ transmission.
Note: To enable CAN (data or remote) frame reception, bit RXEN must be set. For example, if RXEN=’0’ in a TX
message object (DIR=’1’) then a remote frame from CAN bus can not be restored in this object.
Software handling of a transmit message objct
Figure 10 demonstrates the software handling of a transmit (TX) message object (DIR=’1’).
If automatic handling is requested, bit TXEN0 must be initialized with ‘1’.
Together with TXEN1=1, the data transmission is started when flag TXRQ has been set by the hardware
because a received remote frame has a matching identifier."
My understanding is need to set the RXEN = 1 and TXEN0 = 1 for the TX message object to enable its remote-frame-reception and data-transmission. While I haven't seen an clear walkthrough or an example scripts on this.
Appreciate if can shed some light on this.
Regards,
Wei
Show Less
Hello,
how can I use more then one IP on a netif?
adding a netif to the same i cannot figure out...
Is there any example for the XMC4700-F144K2048 AA
In my case I have to use 10.57.0.33 and 10.57.2.33 (mask 255.255.0.0) at the same time!
Thank you for help!!
Wolfgang
Hello ,
Puzzled by the ' No connection' of the new/2nd spin PCB's w/XMC4800F144 .
Have a 1st spin PCB ...no problem connecting and flashing
2nd spin PCB ... problem connecting
O scope shows data looks good (SI) ..some over/undershoot on the clock but within limits
Hooked up SWD Protocol analyzer and investigated bits : appears there is No Acknowledgement during the initial
communication to receive the following:
WData 0x2BA01477 reg IDCODE bits DESIGNER=0x477, PARTNO=0xBA01, Version=0x2 ( 1st spin PCB only)
Prior to aborting connection (2nd spin PCB), request for the following: Request AccessPort Read RAZ_WI
and was acknowledged and provided the following : WData 0x00007800 reg RAZ_WI
Request DebugPort Write ABORT
and was acknowledged and provided the following : WData 0x3FA90000 reg ABORT bits ORUNERRCLR=0, WDERRCLR=0, STKERRCLR=0, STKCMPCLR=0, DAPABORT=0
thank you in advance ..
adam_m
Show Less
Hello,
I compiled a example program for XMC1300 boot kit. I was able to do the debugging part - reading memory and registers.
Suddenly I am getting this below error now and I am not able to do anything on the board.
I have tried to connect the board with XMC_Flasher and Infineon Memtool 2021 both, but the board is not getting connected.
Please guide me for this issue.
Thanks
Show LessI am unable to extract Raw data by using Position2 Go Radar kit in the MATLAB.
MATLAB ERROR:
Error using serial (line 99)
Invalid PORT specified.
Error in RadarSystem (line 10)
obj.hSerialPort = serial(sPortName);
Error in extract_raw_data (line 46)
oRS = RadarSystem(szPort); % setup object and connect to board
Please help me how I can resolve this problem.
Show Less只需要将ICC_CH0_EvalBoard.macro文件中的数据通过spi传输就可以吗?还有没有其他需要设置的地方以及arduino和92464评估板连接是否有什么值得注意的地方。
Dear Sir,
we are running this reference design of 850w ups project.
since this demonstration board is 230VAC input. if I would like to change to 110VAC. may I know how to revise the related parameters of XMC XMC1301?
thanks.
Show LessHi, 我按照guide的要求安装MTBv3.1并配置环境变量,并运行脚本ModusToolbox_URL_Modifier-main,但新建工程尝试一直失败,LOG 如下:
2023/08/19 17:00:05 DEBUG: Log file(s) for this session are stored at: C:\Users\DELL\AppData\Local\Temp\Logs12978806588851258698
2023/08/19 17:00:06 INFO: Launch refreshed on Window Activated event.
2023/08/19 17:01:42 DEBUG: Tools path set from system preference: C:\Users\DELL\ModusToolbox\tools_3.1.
2023/08/19 17:01:42 DEBUG: Transitioning tools from null ==> C:\Users\DELL\ModusToolbox\tools_3.1
2023/08/19 17:01:42 DEBUG: Rebuilding tools resolver for C:\Users\DELL\ModusToolbox\tools_3.1.
2023/08/19 17:01:42 DEBUG: Tools path set from system preference: C:\Users\DELL\ModusToolbox\tools_3.1.
2023/08/19 17:01:42 DEBUG: Transitioning tools from C:\Users\DELL\ModusToolbox\tools_3.1 ==> C:\Users\DELL\ModusToolbox\tools_3.1
2023/08/19 17:01:42 DEBUG: getToolsPath returning: CyRsltOrErr{Value: C:\Users\DELL\ModusToolbox\tools_3.1}.
2023/08/19 17:01:42 DEBUG: CyMakeRunner resolving C:\Users\DELL\ModusToolbox\tools_3.1 with modus-shell and bin
2023/08/19 17:01:42 DEBUG: Tools path set from system preference: C:\Users\DELL\ModusToolbox\tools_3.1.
2023/08/19 17:01:42 DEBUG: getToolsPath returning: CyRsltOrErr{Value: C:\Users\DELL\ModusToolbox\tools_3.1}.
2023/08/19 17:01:42 DEBUG: CyMakeRunner resolving C:\Users\DELL\ModusToolbox\tools_3.1 with modus-shell and bin
2023/08/19 17:01:42 INFO: Running make...
2023/08/19 17:01:42 INFO: C:\Users\DELL\ModusToolbox\tools_3.1\modus-shell\bin\make -f get_tool_info.mk get_tool_info CY_MAKE_IDE=eclipse CY_MAKE_IDE_VERSION=3.1
2023/08/19 17:01:44 INFO: C:/Users/DELL/ModusToolbox/tools_3.1/mtbquery/mtbquery --alltools @MTB_TOOLS_DIR=C:/Users/DELL/ModusToolbox/tools_3.1
2023/08/19 17:01:44 INFO: CY_TOOL_append_to_intel_hex_BASE=airoc-tools/AppendToIntelHex
2023/08/19 17:01:44 INFO: CY_TOOL_append_to_intel_hex_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/airoc-tools/AppendToIntelHex
2023/08/19 17:01:44 INFO: CY_TOOL_append_to_intel_hex_EXE=airoc-tools/AppendToIntelHex/bin/AppendToIntelHex.exe
2023/08/19 17:01:44 INFO: CY_TOOL_append_to_intel_hex_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/airoc-tools/AppendToIntelHex/bin/AppendToIntelHex.exe
2023/08/19 17:01:44 INFO: CY_TOOL_cgs_BASE=airoc-tools/cgs
2023/08/19 17:01:44 INFO: CY_TOOL_cgs_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/airoc-tools/cgs
2023/08/19 17:01:44 INFO: CY_TOOL_cgs_EXE=airoc-tools/cgs/bin/cgs.exe
2023/08/19 17:01:44 INFO: CY_TOOL_cgs_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/airoc-tools/cgs/bin/cgs.exe
2023/08/19 17:01:44 INFO: CY_TOOL_head_or_tail_BASE=airoc-tools/HeadOrTail
2023/08/19 17:01:44 INFO: CY_TOOL_head_or_tail_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/airoc-tools/HeadOrTail
2023/08/19 17:01:44 INFO: CY_TOOL_head_or_tail_EXE=airoc-tools/HeadOrTail/bin/HeadOrTail.exe
2023/08/19 17:01:44 INFO: CY_TOOL_head_or_tail_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/airoc-tools/HeadOrTail/bin/HeadOrTail.exe
2023/08/19 17:01:44 INFO: CY_TOOL_intel_hex_merge_BASE=airoc-tools/IntelHexMerge
2023/08/19 17:01:44 INFO: CY_TOOL_intel_hex_merge_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/airoc-tools/IntelHexMerge
2023/08/19 17:01:44 INFO: CY_TOOL_intel_hex_merge_EXE=airoc-tools/IntelHexMerge/bin/IntelHexMerge.exe
2023/08/19 17:01:44 INFO: CY_TOOL_intel_hex_merge_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/airoc-tools/IntelHexMerge/bin/IntelHexMerge.exe
2023/08/19 17:01:44 INFO: CY_TOOL_intel_hex_to_bin_BASE=airoc-tools/IntelHexToBin
2023/08/19 17:01:44 INFO: CY_TOOL_intel_hex_to_bin_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/airoc-tools/IntelHexToBin
2023/08/19 17:01:44 INFO: CY_TOOL_intel_hex_to_bin_EXE=airoc-tools/IntelHexToBin/bin/IntelHexToBin.exe
2023/08/19 17:01:44 INFO: CY_TOOL_intel_hex_to_bin_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/airoc-tools/IntelHexToBin/bin/IntelHexToBin.exe
2023/08/19 17:01:44 INFO: CY_TOOL_intel_hex_to_hcd_BASE=airoc-tools/IntelHexToHCD
2023/08/19 17:01:44 INFO: CY_TOOL_intel_hex_to_hcd_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/airoc-tools/IntelHexToHCD
2023/08/19 17:01:44 INFO: CY_TOOL_intel_hex_to_hcd_EXE=airoc-tools/IntelHexToHCD/bin/IntelHexToHCD.exe
2023/08/19 17:01:44 INFO: CY_TOOL_intel_hex_to_hcd_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/airoc-tools/IntelHexToHCD/bin/IntelHexToHCD.exe
2023/08/19 17:01:44 INFO: CY_TOOL_shift_intel_hex_BASE=airoc-tools/ShiftIntelHex
2023/08/19 17:01:44 INFO: CY_TOOL_shift_intel_hex_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/airoc-tools/ShiftIntelHex
2023/08/19 17:01:44 INFO: CY_TOOL_shift_intel_hex_EXE=airoc-tools/ShiftIntelHex/bin/ShiftIntelHex.exe
2023/08/19 17:01:44 INFO: CY_TOOL_shift_intel_hex_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/airoc-tools/ShiftIntelHex/bin/ShiftIntelHex.exe
2023/08/19 17:01:44 INFO: CY_TOOL_bsp-assistant_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/bsp-assistant
2023/08/19 17:01:44 INFO: CY_TOOL_bsp-assistant_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/bsp-assistant/bsp-assistant.exe
2023/08/19 17:01:44 INFO: CY_TOOL_bsp-assistant-cli_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/bsp-assistant/bsp-assistant-cli.exe
2023/08/19 17:01:44 INFO: CY_TOOL_bt-configurator_BASE=bt-configurator
2023/08/19 17:01:44 INFO: CY_TOOL_bt-configurator_EXE=bt-configurator/bt-configurator.exe
2023/08/19 17:01:44 INFO: CY_TOOL_bt-configurator-cli_EXE=bt-configurator/bt-configurator-cli.exe
2023/08/19 17:01:44 INFO: CY_TOOL_capsense-configurator_BASE=capsense-configurator
2023/08/19 17:01:44 INFO: CY_TOOL_capsense-tuner_BASE=capsense-configurator
2023/08/19 17:01:44 INFO: CY_TOOL_capsense-configurator_EXE=capsense-configurator/capsense-configurator.exe
2023/08/19 17:01:44 INFO: CY_TOOL_capsense-tuner_EXE=capsense-configurator/capsense-tuner.exe
2023/08/19 17:01:44 INFO: CY_TOOL_capsense-configurator-cli_EXE=capsense-configurator/capsense-configurator-cli.exe
2023/08/19 17:01:44 INFO: CY_TOOL_chipload_BASE=chipload
2023/08/19 17:01:44 INFO: CY_TOOL_chipload_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/chipload
2023/08/19 17:01:44 INFO: CY_TOOL_chipload_EXE=chipload/bin/ChipLoad.exe
2023/08/19 17:01:44 INFO: CY_TOOL_chipload_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/chipload/bin/ChipLoad.exe
2023/08/19 17:01:44 INFO: CY_TOOL_cymcuelftool_BASE=cymcuelftool-1.0
2023/08/19 17:01:44 INFO: CY_TOOL_cymcuelftool_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/cymcuelftool-1.0
2023/08/19 17:01:44 INFO: CY_TOOL_cymcuelftool_EXE=cymcuelftool-1.0/bin/cymcuelftool.exe
2023/08/19 17:01:44 INFO: CY_TOOL_cymcuelftool_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/cymcuelftool-1.0/bin/cymcuelftool.exe
2023/08/19 17:01:44 INFO: CY_TOOL_dashboard_BASE=dashboard
2023/08/19 17:01:44 INFO: CY_TOOL_dashboard_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/dashboard
2023/08/19 17:01:44 INFO: CY_TOOL_dashboard_EXE=dashboard/dashboard.exe
2023/08/19 17:01:44 INFO: CY_TOOL_dashboard_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/dashboard/dashboard.exe
2023/08/19 17:01:44 INFO: CY_TOOL_det_and_id_BASE=detectandid
2023/08/19 17:01:44 INFO: CY_TOOL_det_and_id_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/detectandid
2023/08/19 17:01:44 INFO: CY_TOOL_det_and_id_EXE=detectandid/bin/DetAndId.exe
2023/08/19 17:01:44 INFO: CY_TOOL_det_and_id_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/detectandid/bin/DetAndId.exe
2023/08/19 17:01:44 INFO: CY_TOOL_device-configurator_BASE=device-configurator
2023/08/19 17:01:44 INFO: CY_TOOL_device-configurator_EXE=device-configurator/device-configurator.exe
2023/08/19 17:01:44 INFO: CY_TOOL_device-configurator-cli_EXE=device-configurator/device-configurator-cli.exe
2023/08/19 17:01:44 INFO: CY_TOOL_dfuh-tool_BASE=dfuh-tool
2023/08/19 17:01:44 INFO: CY_TOOL_dfuh-tool_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/dfuh-tool
2023/08/19 17:01:44 INFO: CY_TOOL_dfuh-tool_EXE=dfuh-tool/dfuh-tool.exe
2023/08/19 17:01:44 INFO: CY_TOOL_dfuh-cli_EXE=dfuh-tool/dfuh-cli.exe
2023/08/19 17:01:44 INFO: CY_TOOL_ez-pd-configurator_BASE=ez-pd-configurator
2023/08/19 17:01:44 INFO: CY_TOOL_ez-pd-configurator_EXE=ez-pd-configurator/ez-pd-configurator.exe
2023/08/19 17:01:44 INFO: CY_TOOL_ez-pd-configurator-cli_EXE=ez-pd-configurator/ez-pd-configurator-cli.exe
2023/08/19 17:01:44 INFO: CY_TOOL_fw-loader_BASE=fw-loader
2023/08/19 17:01:44 INFO: CY_TOOL_fw-loader_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/fw-loader
2023/08/19 17:01:44 INFO: CY_TOOL_fw-loader_EXE=fw-loader/bin/fw-loader.exe
2023/08/19 17:01:44 INFO: CY_TOOL_fw-loader_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/fw-loader/bin/fw-loader.exe
2023/08/19 17:01:44 INFO: CY_TOOL_gcc_BASE=gcc
2023/08/19 17:01:44 INFO: CY_TOOL_gcc_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/gcc
2023/08/19 17:01:44 INFO: CY_TOOL_arm-none-eabi-gcc_EXE=gcc/bin/arm-none-eabi-gcc.exe
2023/08/19 17:01:44 INFO: CY_TOOL_arm-none-eabi-gcc_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/gcc/bin/arm-none-eabi-gcc.exe
2023/08/19 17:01:44 INFO: CY_TOOL_arm-none-eabi-g++_EXE=gcc/bin/arm-none-eabi-g++.exe
2023/08/19 17:01:44 INFO: CY_TOOL_arm-none-eabi-g++_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/gcc/bin/arm-none-eabi-g++.exe
2023/08/19 17:01:44 INFO: CY_TOOL_arm-none-eabi-ar_EXE=gcc/bin/arm-none-eabi-ar.exe
2023/08/19 17:01:44 INFO: CY_TOOL_arm-none-eabi-ar_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/gcc/bin/arm-none-eabi-ar.exe
2023/08/19 17:01:44 INFO: CY_TOOL_arm-none-eabi-gdb_EXE=gcc/bin/arm-none-eabi-gdb.exe
2023/08/19 17:01:44 INFO: CY_TOOL_arm-none-eabi-gdb_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/gcc/bin/arm-none-eabi-gdb.exe
2023/08/19 17:01:44 INFO: CY_TOOL_arm-none-eabi-objcopy_EXE=gcc/bin/arm-none-eabi-objcopy.exe
2023/08/19 17:01:44 INFO: CY_TOOL_arm-none-eabi-objcopy_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/gcc/bin/arm-none-eabi-objcopy.exe
2023/08/19 17:01:44 INFO: CY_TOOL_arm-none-eabi-readelf_EXE=gcc/bin/arm-none-eabi-readelf.exe
2023/08/19 17:01:44 INFO: CY_TOOL_arm-none-eabi-readelf_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/gcc/bin/arm-none-eabi-readelf.exe
2023/08/19 17:01:44 INFO: CY_TOOL_kp-firmware_BASE=kp-firmware
2023/08/19 17:01:44 INFO: CY_TOOL_kp-firmware_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/kp-firmware
2023/08/19 17:01:44 INFO: CY_TOOL_lcs-manager-cli_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/lcs-manager-cli
2023/08/19 17:01:44 INFO: CY_TOOL_lcs-manager-cli_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/lcs-manager-cli/lcs-manager-cli.exe
2023/08/19 17:01:44 INFO: CY_TOOL_library-manager-cli_EXE=library-manager/library-manager-cli.exe
2023/08/19 17:01:44 INFO: CY_TOOL_library-manager_BASE=library-manager
2023/08/19 17:01:44 INFO: CY_TOOL_library-manager_EXE=library-manager/library-manager.exe
2023/08/19 17:01:44 INFO: CY_TOOL_lin-configurator_BASE=lin-configurator
2023/08/19 17:01:44 INFO: CY_TOOL_lin-configurator_EXE=lin-configurator/lin-configurator.exe
2023/08/19 17:01:44 INFO: CY_TOOL_lin-configurator-cli_EXE=lin-configurator/lin-configurator-cli.exe
2023/08/19 17:01:44 INFO: CY_TOOL_mbtp_BASE=mbtp
2023/08/19 17:01:44 INFO: CY_TOOL_mbtp_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/mbtp
2023/08/19 17:01:44 INFO: CY_TOOL_mbtp_EXE=mbtp/bin/MbtP.exe
2023/08/19 17:01:44 INFO: CY_TOOL_mbtp_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/mbtp/bin/MbtP.exe
2023/08/19 17:01:44 INFO: CY_TOOL_modus-shell_BASE=modus-shell
2023/08/19 17:01:44 INFO: CY_TOOL_modus-shell_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/modus-shell
2023/08/19 17:01:44 INFO: CY_TOOL_getlibs_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/mtbgetlibs
2023/08/19 17:01:44 INFO: CY_TOOL_getlibs_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/mtbgetlibs/mtbgetlibs.exe
2023/08/19 17:01:44 INFO: CY_TOOL_mtbideexport_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/mtbideexport
2023/08/19 17:01:44 INFO: CY_TOOL_mtbideexport_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/mtbideexport/mtbideexport.exe
2023/08/19 17:01:44 INFO: CY_TOOL_mtbideexport_EXPORT_INTERFACE=3.1
2023/08/19 17:01:44 INFO: CY_TOOL_mtblaunch_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/mtblaunch
2023/08/19 17:01:44 INFO: CY_TOOL_mtblaunch_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/mtblaunch/mtblaunch.exe
2023/08/19 17:01:44 INFO: CY_TOOL_mtbsearch_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/mtbsearch
2023/08/19 17:01:44 INFO: CY_TOOL_mtbsearch_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/mtbsearch/mtbsearch.exe
2023/08/19 17:01:44 INFO: CY_TOOL_openocd_BASE=openocd
2023/08/19 17:01:44 INFO: CY_TOOL_openocd_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/openocd
2023/08/19 17:01:44 INFO: CY_TOOL_openocd_EXE=openocd/bin/openocd.exe
2023/08/19 17:01:44 INFO: CY_TOOL_openocd_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/openocd/bin/openocd.exe
2023/08/19 17:01:44 INFO: CY_TOOL_openocd_scripts_SCRIPT=openocd/scripts
2023/08/19 17:01:44 INFO: CY_TOOL_openocd_scripts_SCRIPT_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/openocd/scripts
2023/08/19 17:01:44 INFO: CY_TOOL_project-creator-cli_EXE=project-creator/project-creator-cli.exe
2023/08/19 17:01:44 INFO: CY_TOOL_project-creator-cli_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/project-creator/project-creator-cli.exe
2023/08/19 17:01:44 INFO: CY_TOOL_project-creator_BASE=project-creator
2023/08/19 17:01:44 INFO: CY_TOOL_project-creator_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/project-creator
2023/08/19 17:01:44 INFO: CY_TOOL_project-creator_EXE=project-creator/project-creator.exe
2023/08/19 17:01:44 INFO: CY_TOOL_project-creator_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/project-creator/project-creator.exe
2023/08/19 17:01:44 INFO: CY_TOOL_proxy-helper_BASE=proxy-helper
2023/08/19 17:01:44 INFO: CY_TOOL_proxy-helper_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/proxy-helper
2023/08/19 17:01:44 INFO: CY_TOOL_proxy-helper_EXE=proxy-helper/proxy-helper.exe
2023/08/19 17:01:44 INFO: CY_TOOL_proxy-helper_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/proxy-helper/proxy-helper.exe
2023/08/19 17:01:44 INFO: CY_TOOL_python_BASE=python
2023/08/19 17:01:44 INFO: CY_TOOL_python_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/python
2023/08/19 17:01:44 INFO: CY_TOOL_python_EXE=python/python.exe
2023/08/19 17:01:44 INFO: CY_TOOL_python_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/python/python.exe
2023/08/19 17:01:44 INFO: CY_TOOL_cysecuretools_EXE=python/Scripts/cysecuretools.exe
2023/08/19 17:01:44 INFO: CY_TOOL_cysecuretools_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/python/Scripts/cysecuretools.exe
2023/08/19 17:01:44 INFO: CY_TOOL_qspi-configurator_BASE=qspi-configurator
2023/08/19 17:01:44 INFO: CY_TOOL_qspi-configurator_EXE=qspi-configurator/qspi-configurator.exe
2023/08/19 17:01:44 INFO: CY_TOOL_qspi-configurator-cli_EXE=qspi-configurator/qspi-configurator-cli.exe
2023/08/19 17:01:44 INFO: CY_TOOL_secure-policy-configurator_BASE=secure-policy-configurator
2023/08/19 17:01:44 INFO: CY_TOOL_secure-policy-configurator_EXE=secure-policy-configurator/secure-policy-configurator.exe
2023/08/19 17:01:44 INFO: CY_TOOL_seglcd-configurator_BASE=seglcd-configurator
2023/08/19 17:01:44 INFO: CY_TOOL_seglcd-configurator_EXE=seglcd-configurator/seglcd-configurator.exe
2023/08/19 17:01:44 INFO: CY_TOOL_seglcd-configurator-cli_EXE=seglcd-configurator/seglcd-configurator-cli.exe
2023/08/19 17:01:44 INFO: CY_TOOL_smartio-configurator_BASE=smartio-configurator
2023/08/19 17:01:44 INFO: CY_TOOL_smartio-configurator_EXE=smartio-configurator/smartio-configurator.exe
2023/08/19 17:01:44 INFO: CY_TOOL_srec_cat_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/srecord/bin/srec_cat.exe
2023/08/19 17:01:44 INFO: CY_TOOL_srec_cmp_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/srecord/bin/srec_cmp.exe
2023/08/19 17:01:44 INFO: CY_TOOL_srec_info_EXE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/srecord/bin/srec_info.exe
2023/08/19 17:01:44 INFO: CY_TOOL_srecord_BASE_ABS=C:/Users/DELL/ModusToolbox/tools_3.1/srecord
2023/08/19 17:01:44 INFO: CY_TOOL_usbdev-configurator_BASE=usbdev-configurator
2023/08/19 17:01:44 INFO: CY_TOOL_usbdev-configurator_EXE=usbdev-configurator/usbdev-configurator.exe
2023/08/19 17:01:44 INFO: CY_TOOL_usbdev-configurator-cli_EXE=usbdev-configurator/usbdev-configurator-cli.exe
2023/08/19 17:01:44 DEBUG: getToolsPath returning: CyRsltOrErr{Value: C:\Users\DELL\ModusToolbox\tools_3.1\project-creator\project-creator.exe}.
2023/08/19 17:01:44 DEBUG: getVersion - file: C:\Users\DELL\ModusToolbox\tools_3.1\project-creator\version.xml
2023/08/19 17:01:44 DEBUG: Tools path set from system preference: C:\Users\DELL\ModusToolbox\tools_3.1.
2023/08/19 17:01:44 DEBUG: getToolsPath returning: CyRsltOrErr{Value: C:\Users\DELL\ModusToolbox\tools_3.1\project-creator\project-creator.exe}.
2023/08/19 17:01:44 INFO: Opening project creator from C:/Users/DELL/ModusToolbox/tools_3.1/project-creator/project-creator.exe
2023/08/19 17:01:44 INFO: Creating process wrapper with the following commands:
2023/08/19 17:01:44 INFO: C:/Users/DELL/ModusToolbox/tools_3.1/project-creator/project-creator.exe
2023/08/19 17:01:44 INFO: --ide=eclipse
2023/08/19 17:01:44 INFO: --ide-readonly
2023/08/19 17:01:44 INFO: --close
2023/08/19 17:01:44 INFO: --ideVersion
2023/08/19 17:01:44 INFO: 3.1
2023/08/19 17:01:44 INFO: --usedNames
2023/08/19 17:01:44 INFO: ""
2023/08/19 17:01:44 INFO: --location
2023/08/19 17:01:44 INFO: D:/ModusToolboxWorkspace
2023/08/19 17:01:44 INFO: --machine-interface
2023/08/19 17:04:41 INFO: Project Creator raw output:
{
"ide": "eclipse",
"logFileLocation": "D:/ModusToolboxWorkspace/project-creator.log",
"messages": [
],
"projects": [
{
"location": "D:/ModusToolboxWorkspace/CAPSENSE_CSD_Button_Tuning",
"messages": [
{
"text": "there was an error retreiving the asset 'https://github.com/cypresssemiconductorco/core-lib' commit 'release-v1.4.0' - fatal: 'C:/Users/DELL/.modustoolbox/cache/git/https___github.com_cypresssemiconductorco_core-lib/core-lib' does not appear to be a git repository, fatal: Could not read from remote repository., Please make sure you have the correct access rights, and the repository exists., command 'C:/Users/DELL/ModusToolbox/tools_3.1/modus-shell/bin/bash -c git -C D:/ModusToolboxWorkspace/mtb_shared/core-lib/release-v1.4.0 fetch --recurse-submodules=no --tags --force cypress --update-head-ok \"refs/heads/*:refs/heads/*\" --quiet', directory '', child process exited with error code 128",
"type": "error"
},
{
"text": "Project 'CAPSENSE_CSD_Button_Tuning' in application directory 'D:/ModusToolboxWorkspace/CAPSENSE_CSD_Button_Tuning' - the getlibs operation failed",
"type": "error"
}
],
"name": "CAPSENSE_CSD_Button_Tuning",
"status": "failed"
}
],
"toolName": "Project Creator",
"version": 1
}
n==============================
2023/08/19 17:04:41 DEBUG: Project Creator Status:
2023/08/19 17:04:41 INFO: Project: CAPSENSE_CSD_Button_Tuning
2023/08/19 17:04:41 INFO: Location: D:/ModusToolboxWorkspace/CAPSENSE_CSD_Button_Tuning
2023/08/19 17:04:41 ERROR: Status: failed
2023/08/19 17:04:41 INFO: Messages:
2023/08/19 17:04:41 ERROR: [1]: there was an error retreiving the asset 'https://github.com/cypresssemiconductorco/core-lib' commit 'release-v1.4.0' - fatal: 'C:/Users/DELL/.modustoolbox/cache/git/https___github.com_cypresssemiconductorco_core-lib/core-lib' does not appear to be a git repository, fatal: Could not read from remote repository., Please make sure you have the correct access rights, and the repository exists., command 'C:/Users/DELL/ModusToolbox/tools_3.1/modus-shell/bin/bash -c git -C D:/ModusToolboxWorkspace/mtb_shared/core-lib/release-v1.4.0 fetch --recurse-submodules=no --tags --force cypress --update-head-ok "refs/heads/*:refs/heads/*" --quiet', directory '', child process exited with error code 128
2023/08/19 17:04:41 ERROR: [2]: Project 'CAPSENSE_CSD_Button_Tuning' in application directory 'D:/ModusToolboxWorkspace/CAPSENSE_CSD_Button_Tuning' - the getlibs operation failed
2023/08/19 17:04:41 DEBUG:
2023/08/19 17:04:41 DEBUG: Machine Interface:
{
"version": 1,
"ide": "eclipse",
"logFileLocation": "D:/ModusToolboxWorkspace/project-creator.log",
"projects": [
{
"name": "CAPSENSE_CSD_Button_Tuning",
"location": "D:/ModusToolboxWorkspace/CAPSENSE_CSD_Button_Tuning",
"status": "failed",
"messages": [
{
"type": "error",
"text": "there was an error retreiving the asset \u0027https://github.com/cypresssemiconductorco/core-lib\u0027 commit \u0027release-v1.4.0\u0027 - fatal: \u0027C:/Users/DELL/.modustoolbox/cache/git/https___github.com_cypresssemiconductorco_core-lib/core-lib\u0027 does not appear to be a git repository, fatal: Could not read from remote repository., Please make sure you have the correct access rights, and the repository exists., command \u0027C:/Users/DELL/ModusToolbox/tools_3.1/modus-shell/bin/bash -c git -C D:/ModusToolboxWorkspace/mtb_shared/core-lib/release-v1.4.0 fetch --recurse-submodules\u003dno --tags --force cypress --update-head-ok \"refs/heads/*:refs/heads/*\" --quiet\u0027, directory \u0027\u0027, child process exited with error code 128"
},
{
"type": "error",
"text": "Project \u0027CAPSENSE_CSD_Button_Tuning\u0027 in application directory \u0027D:/ModusToolboxWorkspace/CAPSENSE_CSD_Button_Tuning\u0027 - the getlibs operation failed"
}
]
}
],
"messages": [],
"tool": "Project Creator"
}
2023/08/19 17:04:41 WARNING: Unable to import the project: CAPSENSE_CSD_Button_Tuning. Try "Import Existing Application" from the quick-panel. If issues persist, retry project creator.
2023/08/19 17:04:41 WARNING: No new/valid projects found.
2023/08/19 17:04:41 INFO: Launch refreshed on Window Activated event.
请问我还有哪个地方没有做对,导致creat project错误?
谢谢。
Show Less
Hello,
Any way to bring/use 8-pin XMC™ MCU debug connector (SWD,SPD & UART) from 2.54mm to 1.27mm pitch ..
For low-cost volume dense XMC1000 applications, 2.54mm pitch male part interface is quite not justified..
Thanks.