XMC™ Forum Discussions
text.format{('custom.tabs.no.results')}
Hi, I have a question about XMC4800,How to realize CAN OPEN protocol based on XMC4800?
Hi, I am using a low-level resolution Encoder for the control of PMSM, and I have a question, how to calculate the speed accurately based on low-level resolution Encoder?
Show LessNow I will configurate XMC4700 pin, what will be provided by Infineon to make it easy? DAVE IDE? thanks
How to monitor the value of variable real time during running?
Before I click "resume", the value can be seen.
After I click "resume", the value can not be seen.
Show Less
Hi,
xmc7200 development board I use keil burn demo, can read the kernel but can not burn, using MTB compilation without errors can not burn. Why?
Best Regards
Show LessHi, I'm using a XMC4108 processor and want to generate an interrupt when I receive CAN RTR frames. I have this working, but for some reason I need to constantly set the DIR bit of the CAN receive Object or it will reset on its own almost immediately after setting it. I am using CAN_NODE_MO_ClearStatus(HandlePtr1->lmobj_ptr[2], XMC_CAN_MO_SET_STATUS_RX_ENABLE | XMC_CAN_MO_SET_STATUS_MESSAGE_DIRECTION); to set the DIR pin, am I doing that correctly or is there a better more correct way of doing it so I don't to make the call over and over?
Thanks, Rob
Show LessWe are trying to use the virtual COM port with Windows on an XMC4400 Eval board.
Basically we added the USBD_VCOM module in DAVE, and tried many different things in main function, but all with same result.
The processor just hangs in the while(!USBD_VCOM_IsEnumDone()), so USB is never enumerated.
Windows shows a device but after a few seconds Windows reports "Device descriptor request failed".
What could be wrong ?
status = DAVE_Init();
if (status == DAVE_STATUS_FAILURE)
{
XMC_DEBUG(("DAVE Apps initialization failed with status %d\n", status));
while (1U){
}
}
if(USBD_VCOM_Connect() != USBD_VCOM_STATUS_SUCCESS)
{
return -1;
}
while(!USBD_VCOM_IsEnumDone());
Show Less
Hi,
I have a XMC45 Relax Kit and I need to know how to implement Ethernet_Client (UDP, TCP does not matter) communication in ModusToolBox with BSP library.
My target is to control some digital outputs from Ethernet communication via a PC(as a server) to send a command through Ethernet and controlling I/O of XMC.
In addition, I do not know why, when I am creating new application in ModusToolBox with XMC45 Relax kit, "cyhal.h" library is not recognized?
I will be thankful if somebody can help me with a source or samples regarding that implementation.
Best regards,
Mo
Show LessHi, I have got a project working with XMC4700 that does USB Host. I used the project example for the XMC4500 "XMC4500_USBH_MS_Example_V1.0" which writes files to a USB flash drive.
There isn't an APP for USB Host in DAVE 4 so the project example comes with code for USB drivers / libraries.
I also need USB device / USB Comm port, and there is an APP for this in Dave 4 .However when I try and merge the 2 projects HOST and DEVICE the driver code and librarires clash and there are hundres of duplicate define errors. It looks like it will be a "long job" trying to combine the duplicate code / defines, ive tried severval different ways.
Has anyone successfully managed to create a project with both Host and Device using Dave 4? Or can anyone point me in the right direction on the best way to merge?
many thanks
Brendan
Show Less