Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

XMC™ Forum Discussions

wph1995
XMC™
Hello everyone, I will use the MCU XMC1404-F064X0200 AA to design a frequency controller for induction motors, and I noticed that I can generate SPWM ... Show More
wph1995
XMC™
Hello, I've been searching for information on the functions of the pins of an XMC1400, and I didn't think it would be so complicated. I had to read ma... Show More
ndosch
XMC™
Hello Infineon Community I have a few questions about the XMC Pinout Tool. First of all I wanted to ask if the XMC Pinout Tool runs with the free Java... Show More
wanglipeng00000
XMC™

Hi, I am design a PMSM motor controller, and I have a question, Does the PMSM controller need DC-bus ripple compensation? 

paoloz
XMC™
hi I try with xmc4500 Relax Lite cart to receive a string of charapter from Uart with dave project. I use Interrupt function for capture 10 charapter ... Show More
LiZJ
XMC™
EVAL_3K3W_TP_PFC_SIC 测试环境: 1、demo切至逆变模式; 2、AC端接阻性负载(不接ac并网模拟器); 3、DC端输入DC400V电源; 测试结果:AC端无 AC230V 电压输出; 问题:当前demo板的默认软件是否不支持上述的测试环境? 是否可以提供支持上述测试环境的软件... Show More
NA97
XMC™
 I am working on a project using xmc7200 where I have 2 push buttons   5 modes and an OLED.1 button is for navigating through the mode, and another is... Show More
wanglipeng00000
XMC™
Hi, I am designing controller for PMSM, and I have a question, how does the controller adapt to motor parameters variation of PMSM during long time ru... Show More
lila_young
XMC™
Hello expert, How can we set the baud rate to non-constant? in my application, I need to change the UART baud rate according to some scenario.  So the... Show More
victxus
XMC™
Hi all, I need to control  an ADC with the XMC4700 by SPI. My requierements are: Mode = Dual SPI Fs SCLK = 15 MHz Frame periodicity = 1.75 us Theref... Show More