XMC™ Forum Discussions
text.format{('custom.tabs.no.results')}
Dear community members,
离线使用ModusToolbox3.1软件,之前成功建立了Ethernet_TCP_Client的模板程序,但不能成功建立Ethernet_TCP_Server的应用程序
Using the modustoolbox 3.1 software offline, the Ethernet_TCP_Client template program was previously successfully established, but the Ethernet_TCP_Server application was not successfully established
编译出现以下问题:
The following problems occurred with compilation:
"C:\\Users\\Administrator\\ModusToolbox\\tools_3.1\\modus-shell\\bin\\make" CY_MAKE_IDE=eclipse CY_IDE_TOOLS_DIR=C:/Users/Administrator/ModusToolbox/tools_3.1 CY_IDE_BT_TOOLS_DIR= --output-sync -j8 all
Tools Directory: C:/Users/Administrator/ModusToolbox/tools_3.1
Removing .mtbqueryapi file...
Searching installed tools in progress...
Searching installed tools complete
C:/Users/Administrator/ModusToolbox/tools_3.1/make/core_version3/startex-v3.mk:159: *** Libraries: "core-make recipe-make" not found. Run "make getlibs" to ensure all required build and code dependencies are present.. Stop.
"C:/Users/Administrator/ModusToolbox/tools_3.1/modus-shell/bin/make CY_MAKE_IDE=eclipse CY_IDE_TOOLS_DIR=C:/Users/Administrator/ModusToolbox/tools_3.1 CY_IDE_BT_TOOLS_DIR= --output-sync -j8 all" terminated with exit code 2. Build might be incomplete.
13:54:34 Build Failed. 1 errors, 0 warnings. (took 406ms)
我应该怎么做呢,期待答疑。
What should I do ,looking forword to your reply.
#XMC
Show Less
Hi,
How does DAVE Project transfer Keil, and which tool will the xmc series chips use in the future?
Best Regards
你好,
我使用DAVE配置了ACMP0,使用P2.8和P2.9作为输入,P0.10作为输出,比较器ACMP0按预期起效了,但是我在生成的代码里找不到关于P2.8作为ACMP0输入的相关底层配置。我想知道我在DAVE的HW Signal Connections配置的P2.8、P2.9作为ACMP输入的代码在哪里找?我在生成的代码里并没有找到他们有连接起来。工程在附件。
我又去看了XMC1302的Keil的ANACMP例程,里面没有配置IO口,但是寄存器P2_IOCR8的复位值是0,所以IO是作为不激活内部拉器件的直接输入模式,但是他没有和外设连接,那么是不是能作为多个外设的输入? Show LessHello,
I am considering replacing from FM4 to XMC7000.
Would you refer the attached excel file?
Checking Vzt and Vfst, FM4 seems to have smaller errors.
Are the following perceptions correct?
1. FM4 is after offset calibration and XMC7000 is before offset calibration, so the error should be smaller than FM4 after offset calibration.
2. Total error is 8 LSB for the FM4 (after calibration) and ±5 LSB (after calibration) for the XMC7000, so the XMC7000 is more accurate.
Best Regards,
Show LessI am using a stepper motor with the XMC4500 kit connected to a TLE8444 driver. I can rotate the motor in both clockwise and anticlockwise directions in half-step mode. How can I implement PWM for motor speed control in DAVE IDE? Do I need to configure the same GPIO pins that I use for the motor driver interface with the MCU as PWM pins?
Show LessHello,
I'm working with XMC4500 and trying to understand why randomly the system gets to a state where it's lockup and only works again after a power reset.
I have a couple of questions:
1 - When a non-configurable fault is active, will the watchdog still work and reset the XMC?
2 - Is it possible to force a hard fault, mem fault, or bus fault to test the system's behavior when they occur? How can I do it?
3 - What is the good way to treat such faults? It is safe to ignore the faults with just a return; or keep it there with a while(1) in the fault's handler?
3.1 - In this case the watchdog will reset the XMC?
The system can work for days before it gets irresponsive which does not help to find the cause of the lockup.
4 - If there is a fail while loading the apps with the DAVE_Init(), it is safe to keep executing the code and start the watchdog?
Thank you for your help!
Daniel
Show LessHello,
I'm trying to connect to the evaluation boards EVAL_3K3W_BIDI_PSFB and EVAL_3K3W_TP_PFC_SIC, but the GUI does not recognize the boards.
The computer recognizes the XMC Link, and the DEBUG LED is ON, as the manual explains. I already downloaded and installed the latest version of J-Link driver "JLink_Windows_V794a_x86_64".
I don't see any troubleshooting or extra steps to follow in the manual. Could someone tell me what I'm missing here?
Thanks
Show Less