Announcements

Help us improve the Power & Sensing Selection Guide. Share feedback

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

XMC™ Forum Discussions

keith_Anet
XMC™
I found one answer regarding implementing a bootloader over ethernet that didn't actually answer the question. Can an XMC device have the flash progra... Show More
Arundev
XMC™
Hi, We have encountered a problem with the EEPROM emulation of the XMC4200. issues found ------------------- We have allocated 70 bytes of memory us... Show More
Bale
XMC™
Hi everybody,I used the Infineon sample source code and ran it successfully with TWINCAT.I'm starting with the "EtherCAT Conformance Test".I ran the r... Show More
rum
XMC™
Hi XMC comunity, in this postSolved: Re: CCU8 module, drive outputs to passive level, d... - Infineon Developer Communityit was suggesed to stop timer... Show More
Stéphane
XMC™
Hello, I'm using a 32k version of XMC1302 and I'd like to be sure about the available Flash space. I have this information, does 7308 (dec) of the "te... Show More
Marcelo_Macedo1
XMC™
Hi, I'm helping a customer to implement Ethernet connectivity using the XMC4400, but I didn't find code examples to understand the memory (flash and r... Show More
Translation_Bot
XMC™
Please tell me why this GPDSC file generated with Dave cannot be opened after being dragged to the MDK icon on the desktop. Show More
yueer666
XMC™

ADC_MEASUREMENT_StartConversion(&ADC_MEASUREMENT_0); 用XMC1302做AD转换,初始化AD用这个函数,程序就死在这里面,请问这是什么原因?附件是MDK的程序,初始化程序就执行到这个AD初始化就不能往下执行了

elibarber
XMC™
So I flashed the example code to myXMC 1100 bootkit, hoping to connect to it with  my terminal application on PC. Getting no response when I open up a... Show More
bs23
XMC™
Hi, We are using P2.4 (clk) and Pin2.5 (data) on the XMC4800 to communicate with an STM32F427 device.  On some boards, we are not able to get an ack b... Show More