XMC™ Forum Discussions
Hello Infineon,
My team is doing a feasibility study on using the XMC7200 microcontroller for our project. One of the requirement is to have parallel communication between the XMC7200 with external RAM.
My question is that is there an already written XMC7200 Hyperbus driver support for external RAM (parallel memory interface)?
Show LessHello,
what's the relationship between "time interval" in APP configuration and "TIMER_SetTimeInterval" in function?
You can see I have set the "Time interval[usec]" to 1200, and then I use function "TIMER_SetTimeInterval" set to 1.
Then what is the real time interval I have set? After How long time will the "time interval event" be triggered?
Thanks!
Show Less
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/XMC/%E5%A6%82%E4%BD%95%E5%9C%A8%E5%88%AB%E7%9A%84IDE%E4%B8%AD%E4%BF%AE%E6%94%B9%E5%92%8C%E4%BD%BF%E7%94%A8DAVEAPP%E7%94%9F%E6%88%90%E7%9A%84%E5%A4%96%E8%AE%BE%E9%85%8D%E7%BD%AE%E4%BB%A3%E7%A0%81/td-p/500477
Show Less使用XMC4300芯片在Eclipse中创建ethercat的工程,有相应的例程框架吗,还有就是DAVE apps插件应该怎么下载呢,我没有搜索到。打扰了,期待回复
Hello,
I am developing a program that executes the XMC Flasher .exe, and programs a board using said flasher.
However, I would like to be able to program/set BMI of multiple boards at the same time by having multiple programmers connected into my PC. If multiple XMC programmers are connected to my PC at once, is there a way to identify, select, and control a specific programmer, perhaps through the programmer's COM port or serial number?
If not possible through XMC Flasher, is there is other software that would accomplish what I'm trying to do?
Thank you,
Alex
Show LessHI, All
I only look at the following Block diagram. I could not find the full application document. Can someone provide me with a complete document? Thanks!
Show Less
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/XMC/XMC4800-%E4%B8%B2%E5%8F%A3%E4%B8%AD%E6%96%AD%E6%8E%A5%E6%94%B6%E6%95%B0%E6%8D%AE%E9%94%99%E8%AF%AF/td-p/496613
Show LessTake GPIO as an example, after the RTE is configured, there will be xmc_gpio.h, xmc1_gpio.h, xmc_gpio.c, xmc1_gpio.c, what kind of relationship is there among the four? Why is there a declaration of XMC_GPIO_Init in xmc_gpio.h, but no definition of XMC_GPIO_Init in the xmc_gpio.c file?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/XMC/XMC%E7%9A%84RTE%E9%85%8D%E7%BD%AE%E7%9A%84%E7%96%91%E6%83%91/td-p/497237
Show LessCan you tell me how much work it is to port the original PMSM 3-phase motor FOC project made with XMC4700F100K1536 to XMC1404F064X0128AA?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/XMC/%E8%AF%B7%E9%97%AE%E5%8E%9F%E6%9D%A5%E7%94%A8XMC4700F100K1536%E5%81%9A%E7%9A%84PMSM%E4%B8%89%E7%9B%B8%E7%94%B5%E6%9C%BA%E7%9A%84FOC%E5%B7%A5%E7%A8%8B%E7%A7%BB%E6%A4%8D%E5%88%B0XMC1404F064X0128AA%E4%B8%8A%E9%9D%A2-%E5%B7%A5%E4%BD%9C%E9%87%8F%E5%A4%A7%E4%B8%8D%E5%A4%A7/td-p/734102
Show LessHello,
I am trying to use CAN bus XMC 4700 (250kbps), but it has only 32 IDs available on DAVE IDE, could tell me how can I use more than 32 IDs.
Also, I tried using Multican buts its not working properly.