Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

XMC™ Forum Discussions

PrathameshJ
XMC™
Hello, Can we use project (created in DAVE IDE) into Modus toolbox eclipse IDE? If yes, how? If no, why not? BRs, Prathamesh. Show More
TJ__
XMC™
Hi, I wish to use EVAL_TOLT_DC48V_3KW with KIT_XMC1400_DC_V1 driver card instead of XMC1300, but could not find KIT_XMC1400_DC_V1 schematics online. ... Show More
cg7g14
XMC™
I have just joined a company using the XMC4500 chipset. They have legacy products that need maintaining, the code for which was generated using DAVE 3... Show More
Alex8274
XMC™
XMC7000D
solved msg Solved
您好! 1、CAN的发送,架构手册上发送有Tx buffer模式,fifo模式,和queue模式,实际在modusbox的设备配置器里只有Tx buffer模式,应用手册里也没有相关说明。希望能有对应的例程或说明文档。 2,ADC的应用手册AN234282里,设备配置器里的截图和配置代码不一致,无法... Show More
guojun0718
XMC™

英飞凌是否有支持matter协议的开发板?或者mcu吗?

如果没有,英飞凌在智能家居领域有哪些通讯协议?

NA97
XMC™
am attempting to control the speed of a DC stepper motor using an Infineon TLE8444SL motor driver. The four outputs of the driver are connected to th... Show More
Guillermo1
XMC™
Hi, I need to configure an SPI Master for reading frames of 16 bits every 1.75 us =  571.430 KHz. After doing a lot of configuration test the most I a... Show More
Ahlan
XMC™
I am trying to program the XMC4500 Relax board without using Dave or the XMC libraries. Therefore the core and clock setup is my own code. I have prog... Show More
lmariotti
XMC™
Hi everyone, I'm new on XMC4700-F144K2048 AA # but I've a very long story with Infineon SAK-XE167FM-72F80LR AB . For XMC I've builded my own bootloade... Show More
lmariotti
XMC™
Hi everyone that post is a follow-up to:https://community.infineon.com/t5/XMC/XMC4700-USB-HOST/m-p/473093#M13214 I'm looking for an USBH APP for XMC47... Show More