XMC™ Forum Discussions
XMC™
HelloI am really disappointed with Infineon.Few experts answer your queries. Seldom is the problem resolved.This I can say because couple of my roadbl...
Show More
Hello
I am really disappointed with Infineon.
Few experts answer your queries. Seldom is the problem resolved.
This I can say because couple of my roadblocks have sustained.
I have nowhere to go.
Local help and from Infineon Germany is absent.
Dave IDE is buggy.
Maybe Infineon MCU are the wrong choice for us. Show Less
I am really disappointed with Infineon.
Few experts answer your queries. Seldom is the problem resolved.
This I can say because couple of my roadblocks have sustained.
I have nowhere to go.
Local help and from Infineon Germany is absent.
Dave IDE is buggy.
Maybe Infineon MCU are the wrong choice for us. Show Less
XMC™
Hi,I find there is CMSIS_RTOS and FreeRTOS APP in DAVE, if i used FreeRTOS in freescale MCU and want to immigrate to XMC4300, should i add the FreeRTO...
Show More
Hi,
I find there is CMSIS_RTOS and FreeRTOS APP in DAVE, if i used FreeRTOS in freescale MCU and want to immigrate to XMC4300, should i add the FreeRTOS instead of CMSIS_RTOS?
Anu guideline/notes for the imigratation?
Thank you
Regards,
Herry Show Less
I find there is CMSIS_RTOS and FreeRTOS APP in DAVE, if i used FreeRTOS in freescale MCU and want to immigrate to XMC4300, should i add the FreeRTOS instead of CMSIS_RTOS?
Anu guideline/notes for the imigratation?
Thank you
Regards,
Herry Show Less
XMC™
Hi I'm looking for a TCP connection between computer and XMC4700.I’m using the demoboard “KIT_XMC47_RELAX_V1”.With the ETH_LWIP_0 stack and "usage" de...
Show More
Hi
I'm looking for a TCP connection between computer and XMC4700.
I’m using the demoboard “KIT_XMC47_RELAX_V1”.
With the ETH_LWIP_0 stack and "usage" description, I can "ping" me XMC with computer.
I want to transmit some data from computer to microcontroller and vice versa with the Tcp/ip protocol.
The next step for me is to find function to send and receive some data with this protocol. I don't understand the APP very well.
Have you got any idea about function or process permitting to do that?
I heard about Signals or Events to permit the Receiving detection but it's unclear in my mind and I didn't find documentation about that.
Maybe it's easy but I'm not an expert in network connection.
Thanks and have a nice day.
Best regards,
Geoffrey Show Less
I'm looking for a TCP connection between computer and XMC4700.
I’m using the demoboard “KIT_XMC47_RELAX_V1”.
With the ETH_LWIP_0 stack and "usage" description, I can "ping" me XMC with computer.
I want to transmit some data from computer to microcontroller and vice versa with the Tcp/ip protocol.
The next step for me is to find function to send and receive some data with this protocol. I don't understand the APP very well.
Have you got any idea about function or process permitting to do that?
I heard about Signals or Events to permit the Receiving detection but it's unclear in my mind and I didn't find documentation about that.
Maybe it's easy but I'm not an expert in network connection.
Thanks and have a nice day.
Best regards,
Geoffrey Show Less
XMC™
Mời bạn tham khảo ngay Orient FKV01002D0 một trong những cách thức gây ấn tượng sâu sắc ấn tượng. Thế giới ngày càng phát triển người ta sẽ càng ngày ...
Show More
Mời bạn tham khảo ngay Orient FKV01002D0 một trong những cách thức gây ấn tượng sâu sắc ấn tượng. Thế giới ngày càng phát triển người ta sẽ càng ngày phát minh ra những mẫu đồng hồ sang trọng như thế.
--- Tham khảo Đồng hồ Tissot 1853 giá bao nhiêu <-- thông tin chính hãng
Ấn Tượng Sâu Với Mặt Số Orient FKV01002D0
Chân dung Orient FKV01002D0 mặt số xanh
➤ Chi tiết sang trọng nhất của Orient FKV01002D0 chính là mặt số đầy chi tiết cao cấp lại có màu sắc cực kỳ thu hút.
+ Mặt số đồng hồ cao cấp với tấm nền xanh dương có ánh lấp lánh kim loại toát nên sự sang trọng. Đặc biệt các chi tiết như màu xanh cá tính vừa thời trang vừa nam tính. Màu xanh tạo hiệu ứng chiều sâu khiến đồng hồ càng thu hút hơn.
+ Các con số giờ la tinh của đồng hồ có kích thước cực lớn, rõ nét, bản dày có thể phát sáng tốt trong đêm là những chi tiết luôn được xuất hiện trong những chiếc đồng hồ cao cấp.
+ Kim đồng hồ sang trọng bằng thép không gỉ cao cấp có tích hợp dạ quang phát sáng trong đêm.
+ Đồng hồ có bộ 3 đồng hồ mặt số phụ cho các chức năng chronograph chuyên nghiệp, thể hiện tinh thần thể thao nam tính, góp phần làm cho mặt số ấn tượng hơn.
➤ Nhận xét chung về mặt số: Với phong cách ấn tượng nền số xanh sang trọng chúng ta có các chi tiết vô cùng đa dạng khác trên mặt số như con số, vạch số và các chi tiết khác nữa. Mặt số Đồng hồ đeo tay đẹp giá rẻ Orient FKV01002D0 nhìn chung bị tràn đầy các khí phái nam nhi cao cấp, mặt số phức tạp, chằng chịt chi tiết nhưng là cố tình để thể hiện sự chuyên nghiệp, đa dạng chức năng của mặt số
Hộp đồng hồ Orient chính hãng
Thông Tin Khác Về Thiết Kế Orient FKV01002D0
> Mặt số của Orient FKV01002D0 có kích thước rộng lớn, bán kính to, đường viền mặt số lẫn khung niềng lớn, uy nghi để bảo vệ bộ máy bên trong.
> Đường viền khung niềng có các hình răng cưa cao cấp thể hiện phong độ cách điệu, tạo sức hút cho đồng hồ thể thao.
> Cả bộ vỏ của Orient FKV01002D0 dày dặn mạnh mẽ, có màu bạc kim loại sang trọng theo phong cách nam tính thanh lịch. Kết cấu của bộ vỏ lại càng đơn giản và thu hút phái mạnh.
Tham Khảo Thông Tin Khác
Thương Hiệu: Orient
Số Hiệu Sản Phẩm: FKV01002D0
Xuất Xứ: Nhật Bản
Giới Tính: Nam
Kính: Mineral Crystal (Kính Cứng)
Máy: Quartz (Pin)
Bảo Hành Quốc Tế: 1 Năm
Bảo Hành Tại Hải Triều: 5 Năm
Đường Kính Mặt Số: 45 mm
Bề Dày Mặt Số: 10 mm
Niềng: Thép Không Gỉ
Dây Đeo: Thép Không Gỉ
Màu Mặt Số: Xanh
Chống Nước: 5 ATM
Chức Năng: Lịch Ngày – Đồng Hồ 24 Giờ – Chronograph
Tham Khảo Ngay
Đồng hồ Hải Triều là nơi có gần 25 kinh nghiệm trong kinh doanh đồng hồ, tại đây bán hơn 26 thương hiệu và trên 3000 mẫu Đồng hồ thời trang giá rẻ tại tphcm nam nữ - một thiên đường mua sắm đa dạng
➤ Chưa dùng lại ở đó, Hải Triều còn có những chế độ quyền lợi khác dành cho khách hàng:
>> Đổi hàng miễn phí trong vòng 7 ngày – cho đồng hồ chưa có dấu hiệu sử dụng hoặc do lỗi của nhà sản xuất.
>> Giao hàng tận nhà và thanh toán tận nhà cho khách hàng có nhu cầu
>> Cam kết đền 10 lần nếu phát hiện hàng nhái, hàng giả.
--- Tham khảo Đồng hồ Tissot 1853 giá bao nhiêu <-- thông tin chính hãng
Ấn Tượng Sâu Với Mặt Số Orient FKV01002D0
Chân dung Orient FKV01002D0 mặt số xanh
➤ Chi tiết sang trọng nhất của Orient FKV01002D0 chính là mặt số đầy chi tiết cao cấp lại có màu sắc cực kỳ thu hút.
+ Mặt số đồng hồ cao cấp với tấm nền xanh dương có ánh lấp lánh kim loại toát nên sự sang trọng. Đặc biệt các chi tiết như màu xanh cá tính vừa thời trang vừa nam tính. Màu xanh tạo hiệu ứng chiều sâu khiến đồng hồ càng thu hút hơn.
+ Các con số giờ la tinh của đồng hồ có kích thước cực lớn, rõ nét, bản dày có thể phát sáng tốt trong đêm là những chi tiết luôn được xuất hiện trong những chiếc đồng hồ cao cấp.
+ Kim đồng hồ sang trọng bằng thép không gỉ cao cấp có tích hợp dạ quang phát sáng trong đêm.
+ Đồng hồ có bộ 3 đồng hồ mặt số phụ cho các chức năng chronograph chuyên nghiệp, thể hiện tinh thần thể thao nam tính, góp phần làm cho mặt số ấn tượng hơn.
➤ Nhận xét chung về mặt số: Với phong cách ấn tượng nền số xanh sang trọng chúng ta có các chi tiết vô cùng đa dạng khác trên mặt số như con số, vạch số và các chi tiết khác nữa. Mặt số Đồng hồ đeo tay đẹp giá rẻ Orient FKV01002D0 nhìn chung bị tràn đầy các khí phái nam nhi cao cấp, mặt số phức tạp, chằng chịt chi tiết nhưng là cố tình để thể hiện sự chuyên nghiệp, đa dạng chức năng của mặt số
Hộp đồng hồ Orient chính hãng
Thông Tin Khác Về Thiết Kế Orient FKV01002D0
> Mặt số của Orient FKV01002D0 có kích thước rộng lớn, bán kính to, đường viền mặt số lẫn khung niềng lớn, uy nghi để bảo vệ bộ máy bên trong.
> Đường viền khung niềng có các hình răng cưa cao cấp thể hiện phong độ cách điệu, tạo sức hút cho đồng hồ thể thao.
> Cả bộ vỏ của Orient FKV01002D0 dày dặn mạnh mẽ, có màu bạc kim loại sang trọng theo phong cách nam tính thanh lịch. Kết cấu của bộ vỏ lại càng đơn giản và thu hút phái mạnh.
Tham Khảo Thông Tin Khác
Thương Hiệu: Orient
Số Hiệu Sản Phẩm: FKV01002D0
Xuất Xứ: Nhật Bản
Giới Tính: Nam
Kính: Mineral Crystal (Kính Cứng)
Máy: Quartz (Pin)
Bảo Hành Quốc Tế: 1 Năm
Bảo Hành Tại Hải Triều: 5 Năm
Đường Kính Mặt Số: 45 mm
Bề Dày Mặt Số: 10 mm
Niềng: Thép Không Gỉ
Dây Đeo: Thép Không Gỉ
Màu Mặt Số: Xanh
Chống Nước: 5 ATM
Chức Năng: Lịch Ngày – Đồng Hồ 24 Giờ – Chronograph
Tham Khảo Ngay
Đồng hồ Hải Triều là nơi có gần 25 kinh nghiệm trong kinh doanh đồng hồ, tại đây bán hơn 26 thương hiệu và trên 3000 mẫu Đồng hồ thời trang giá rẻ tại tphcm nam nữ - một thiên đường mua sắm đa dạng
➤ Chưa dùng lại ở đó, Hải Triều còn có những chế độ quyền lợi khác dành cho khách hàng:
>> Đổi hàng miễn phí trong vòng 7 ngày – cho đồng hồ chưa có dấu hiệu sử dụng hoặc do lỗi của nhà sản xuất.
>> Giao hàng tận nhà và thanh toán tận nhà cho khách hàng có nhu cầu
>> Cam kết đền 10 lần nếu phát hiện hàng nhái, hàng giả.
JIKTAM
Show Less
XMC™
New user to DAVE here. I have an application where I want to need GPIO control of a pin and then later use that pin for PWM output. Can I do this wi...
Show More
New user to DAVE here. I have an application where I want to need GPIO control of a pin and then later use that pin for PWM output. Can I do this with APP's or do I have to program this at a lower level?
I am using an XMC2go board for testing.
--john Show Less
I am using an XMC2go board for testing.
--john Show Less
XMC™
Today I released version 1.3.0 of the open source OpenBLT bootloader. In addition to the XMC4000 family, it now features support for the XMC1000 famil...
Show More
Today I released version 1.3.0 of the open source OpenBLT bootloader. In addition to the XMC4000 family, it now features support for the XMC1000 family.
The bootloader package contains a demo for the XMC1400 Boot Kit, which supports firmware updates via UART and CAN. Download is available from https://www.feaser.com.
Feedback and ideas are always welcome!
-Frank Show Less
The bootloader package contains a demo for the XMC1400 Boot Kit, which supports firmware updates via UART and CAN. Download is available from https://www.feaser.com.
Feedback and ideas are always welcome!
-Frank Show Less
XMC™
I am using tm4c123g and ds1307 to display time (hh:mm:ss) on sevensegments and date and day on lcd(16x2). IS there any way way to use same 8 pins for ...
Show More
I am using tm4c123g and ds1307 to display time (hh:mm:ss) on sevensegments and date and day on lcd(16x2).
IS there any way way to use same 8 pins for data of both (lcd and seven segment display..as they are to diplay different data).
Can time multiplexing be used for that purpose? Tell me any idea or any way to do this... Show Less
IS there any way way to use same 8 pins for data of both (lcd and seven segment display..as they are to diplay different data).
Can time multiplexing be used for that purpose? Tell me any idea or any way to do this... Show Less
XMC™
HelloI am trying to use emWin with XMC4500-F100x1024.The Flash size for this MCU is 1Mb and RAM size is 160k.My Display is 800x480 , and my driver is ...
Show More
Hello
I am trying to use emWin with XMC4500-F100x1024.
The Flash size for this MCU is 1Mb and RAM size is 160k.
My Display is 800x480 , and my driver is SSD1963 in 16-bit parallel RGB565 mode.
I am having troubles with the emWin library which I have posted elsewhere.
On my board I have a QSPI N25Q032 from Micron as an external flash.
My Goal :
I want to store all images, Fonts and any memory hungry resources required by emWin to this Flash.
EmWin should fetch these images/fonts/gif etc. from the Flash and draw them to the TFT.
What I can achieve till now:
I can read and write to the flash in 256 byte page size and read it, but all values are hex values.
Problem statement:
EmWin requires images which it renders, stored as a C-file, included at compile time in local flash.
I use BMPconvert images to C-files.
I include these files and I have no problem drawing these on the TFT.
I am planning to store these images to the external flash during run time over a USB communication interface of XMC4500. A Windows based software will talk with the XMC4500 for this.
I know how to transfer data over USB, but unsure how to transfer a C-file likewise.
I don’t know how emWin would fetch this data from the external flash at runtime.
EmWin requires more RAM, it seems since most of transparency, multilayer and alpha blending functions have never worked for me.
In the GUI_SEGGERLIBRARY app, if I enable the cache for non-readable display, emWin crashes. Perhaps there is insufficient memory.
I am trying to use GUI_DrawStreamedBitmap() but not able to understand how it can used in my case where the data to be streamed is under another protocol layer (QSPI).
I have been running from pillar to post but unable to understand or resolve this.
Please help me. Show Less
I am trying to use emWin with XMC4500-F100x1024.
The Flash size for this MCU is 1Mb and RAM size is 160k.
My Display is 800x480 , and my driver is SSD1963 in 16-bit parallel RGB565 mode.
I am having troubles with the emWin library which I have posted elsewhere.
On my board I have a QSPI N25Q032 from Micron as an external flash.
My Goal :
I want to store all images, Fonts and any memory hungry resources required by emWin to this Flash.
EmWin should fetch these images/fonts/gif etc. from the Flash and draw them to the TFT.
What I can achieve till now:
I can read and write to the flash in 256 byte page size and read it, but all values are hex values.
Problem statement:
EmWin requires images which it renders, stored as a C-file, included at compile time in local flash.
I use BMPconvert images to C-files.
I include these files and I have no problem drawing these on the TFT.
I am planning to store these images to the external flash during run time over a USB communication interface of XMC4500. A Windows based software will talk with the XMC4500 for this.
I know how to transfer data over USB, but unsure how to transfer a C-file likewise.
I don’t know how emWin would fetch this data from the external flash at runtime.
EmWin requires more RAM, it seems since most of transparency, multilayer and alpha blending functions have never worked for me.
In the GUI_SEGGERLIBRARY app, if I enable the cache for non-readable display, emWin crashes. Perhaps there is insufficient memory.
I am trying to use GUI_DrawStreamedBitmap() but not able to understand how it can used in my case where the data to be streamed is under another protocol layer (QSPI).
I have been running from pillar to post but unable to understand or resolve this.
Please help me. Show Less
XMC™
Hi,I have read the reference manual in order to understand if it's possible to set up the USIC module on a XMC4500 for RS232 with flow control "RTS/CT...
Show More
Hi,
I have read the reference manual in order to understand if it's possible to set up the USIC module on a XMC4500 for RS232 with flow control "RTS/CTS (RTR/CTS)". However, I not been able to understand whether it's possible or not so I would really appreciate some hints here. Hopefully somebody has experience from a similar setup or other useful information..?
For instance:
- Can DX1/DX2 stages be used for "CTS"?
- How can I generate a "RTR"?
Best regards,
Johan Show Less
I have read the reference manual in order to understand if it's possible to set up the USIC module on a XMC4500 for RS232 with flow control "RTS/CTS (RTR/CTS)". However, I not been able to understand whether it's possible or not so I would really appreciate some hints here. Hopefully somebody has experience from a similar setup or other useful information..?
For instance:
- Can DX1/DX2 stages be used for "CTS"?
- How can I generate a "RTR"?
Best regards,
Johan Show Less
XMC™
Hi,How can i program the EEPROM which connected to EtherCAT slave(XMC4300) from a master side(TwinCAT)?Any example/guideline?:oThank youRegards,Herry
Show More
Hi,
How can i program the EEPROM which connected to EtherCAT slave(XMC4300) from a master side(TwinCAT)?
Any example/guideline?:o
Thank you
Regards,
Herry Show Less
How can i program the EEPROM which connected to EtherCAT slave(XMC4300) from a master side(TwinCAT)?
Any example/guideline?:o
Thank you
Regards,
Herry Show Less