Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

XMC™ Forum Discussions

Sort by:
GarageDirt
XMC™
I have two analog signals in the shape of a gaussian curve having an amplitude of about 500 mv and duration of 20 microseconds.  These pulses happen a... Show More
Yalcin_Haksoz
XMC™
Hi, I am trying to get the FPU going on XMC4200 but for some reason I am not able to get the expected performance. I am using the latest version of DA... Show More
jonatanzeidler
XMC™
The XMCLib EtherCAT abstraction requires the XMC_ECAT_PORT_CTRL_t config struct, which asks for MDIO (SMI) related configs like phyaddr_offset and mdi... Show More
firstgoods
XMC™
我现在写的代码,发送是没有问题的,但是接收的数据存在问题。有时候能正确接收到,有时候不能征求接收到。我发送完数据,对方应该给我返回三个字节的数据。从逻辑分析仪上看是正确的,但是把接收到的数据通过串口发送到电脑,数据和逻辑分析仪上的数据不一致。感觉串口接收buf中的数据没有被清空。另外,没有使用FIF... Show More
lila_young
XMC™
Hello, when I try to import project, sometimes the imported project is not working, it may don't have main.c.   Show More
Ranjitha
XMC™
Dear Team, We have made a CAN circuit with CAN IC part number (SN65HVD230QDRG4Q1) & Controller we are using MCU Part number: XMC4108Q48K64BAXUMA1, But... Show More
Sebastian1
XMC™
Hi, we use the XMC4500 for functional safety applications. There are several user installations with 1000 controller or more. In those field installat... Show More
raad
XMC™
Since I am continuing to work on projects for the XMC4 series I understand that it is recommended to migrate from DAVE IDE to ModusToolbox.Currently t... Show More
PJFIXER
XMC™
Hello everyone, For a project i need to generate a 8mhz PWM with 8bit résolution. Currently i have tried with some ST's product without succes because... Show More
SaAo
XMC™
Hi, All, My customer would like to use VDDD=3.3V and VDDA=5V.The datasheet states the following Am I correct in assuming that this is possible if ADC... Show More