Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

XMC™ Forum Discussions

Alex8274
XMC™
XMC7200d
solved msg Solved
Dear Lingling, 在另外一个帖子里面提供的Demo测试是可以的, 目前存在一个问题,我在例程上更改为PWM触发采样也可以正常运行,例程里用的是adc0,单独触发ADC0正常,但是我增加并更改为触发ADC2就无法正常触发采集,如果同时触发ADC0和ADC2,则两个ADC触发采样都是正常的。... Show More
nDonnelly
XMC™
HI I am getting the following error when trying to debug XMC, note this is happening for half of my boards, and the other half are connecting no probl... Show More
shilchenbach
XMC™
Hello, the XMC4700 Relax USBD MS Bootloader example uses the Infineon USB Vendor ID 0x058B and Product ID 0x0060."Getting Started - XMC4700_Relax_USBD... Show More
Ors
XMC™
Hello, I have the following issue with the UART FIFO buffer. Description of the problem: When using the complete UART FIFO buffer by two UART channels... Show More
Mau5
XMC™
Dear community, I recently hooked up an "XMC4500 Relax Lite Kit-V1" dev-board to my JTAG live controller to get first experiences with boundary scan. ... Show More
user_ah
XMC™
Hi, As title. does any sample code support below use case? IPCam output data over ethernet then rout to wifi(Station mode)  ---> AP router Thanks. Aus... Show More
IronWaffle
XMC™
Good day!I would like to ask if there are LoraWAN Libraries in Arduino IDE that is compatible with the XMC2Go?I am attempting to transmit data via Lor... Show More
DeGu
XMC™
Good Day, I have an issue when using the XMC4500 µC to interface an ADS1278 ADC with the SPI-App. When configured as SPI_MASTER in half-duplex mode I ... Show More
kevinzhang
XMC™
PHD
solved msg Solved

MEMS Microphone

User12255
XMC™
Hello, I am developing an EtherCAT to CANOPEN gateway using XMC4300 EtherCAT relax card. EtherCAT slave code is Beckhoff SSC sample code with no modif... Show More