Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

XMC™ Forum Discussions

kivikkivik
XMC™
Hi,I'm trying to do the led flash when data reaches one and then send the data to the other device. and I want it to patch it in a loop. I have 1 mast... Show More
SmartTommy
XMC™
Hi everybody,So I'm using Dave 4 Apps to implement a Quadrature Encoder and I have no problem with rotor angle. But now I have a problem with Index Ev... Show More
NA97
XMC™
I am trying to use buttons 1.14 and 1.15 both as interrupts to perform specific actions. I can configure only one button as an interrupt using the eve... Show More
lmariotti
XMC™
Hi everyone, I've a project developed with DAVE IDE v4.5.0 targeted for XMC4700F144x2048.I would like to migrate this project to XMC4500F144x1024, I'v... Show More
tezelcelebi
XMC™
Hello, I designed a new board with XMC4700. All work OK but when the card is powered on, it hangs op. Unless I push the reset button, it does not st... Show More
wdc1234
XMC™
I am looking for example code for KIT_XC48_IOT_AWS_WIFI. I want to run a basic ethercat slave. I can't find any code I tried to migrate Relax 144 pin ... Show More
Javiertxo
XMC™
Hi everyone, First of all, thanks to the community for the doubts resolved. This is my first entry, so I hope it is correct and clear. In my case, I n... Show More
Ryu_849312311
XMC™
Dear supporter,   The list of peripherals in the XMC4700 data sheet says "SD and Multi-Media Card interface (SDMMC) for data storage memory cards", bu... Show More
Alex8274
XMC™
XMC7200d
solved msg Solved
Dear Lingling, 在另外一个帖子里面提供的Demo测试是可以的, 目前存在一个问题,我在例程上更改为PWM触发采样也可以正常运行,例程里用的是adc0,单独触发ADC0正常,但是我增加并更改为触发ADC2就无法正常触发采集,如果同时触发ADC0和ADC2,则两个ADC触发采样都是正常的。... Show More
nDonnelly
XMC™
HI I am getting the following error when trying to debug XMC, note this is happening for half of my boards, and the other half are connecting no probl... Show More