Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

XMC™ Forum Discussions

User18523
XMC™
Hello,Am using the XMC4500 relax kit. Now am trying to use CAN from the controller. My basic requirement is to receive some CAN frames from another mo... Show More
User18348
XMC™
Hello,I am very new to using the XMC and Dave environment. I have an XMC 4300 development board and I want to read out the ADC. I have tried examples ... Show More
User18316
XMC™
Hello people!I'm sorry to ask such a stupid question, but I'm stuck. 😞I would like to create a simple delay function (without Dave).Does anyone have ... Show More
User8570
XMC™
HiUsing Dave4, it seems not possible to set the CAN bitrate to 33.3Kbps. i would like to know if it can be achieved? if so, what could be the setting... Show More
User8320
XMC™
Hello.I am looking for POSIF APP on dave4.But I can not find it.I used it as APP in DAVE3.I want to know how to use the POSIF function in DAVE4.I want... Show More
User18496
XMC™
Goodmorning to all.I'm an XMC user, and I'm developing with dave on XMC 4500. I'm using segger Jlink programmer and Infineaon XMC link programmer.I tr... Show More
User18035
XMC™
Hi, we're working on a project built around a XMC4700 with external RAM on EBU bus and need to use a microSD card as memory storage with FatFs.The car... Show More
Anonymous
XMC™
Hi,working on SD card example below http://www.keil.com/appnotes/files/apnt_273.pdfwith different IO pins for SPI Interface of Micro SD card with XMC4... Show More
User14735
XMC™
HelloI am using the XMC 4400 chip and the part which I am going to discuss is part of a larger code. At power up I write certain data into the flash m... Show More
User13630
XMC™
Hi,in the help of BUCK_PCC_FIX_FQ APPThere are two possible sources for an ADC trigger. a. Manual connection:User can connect any other existing time... Show More