Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

XMC™ Forum Discussions

User21562
XMC™
Just downloaded a example dave poject , but the "manual PIN allocator " is not showing any Port pins to select(Its blank)Please help in solving the is... Show More
User21055
XMC™
Hello There,I have a question regarding the support of CAN remote frame with a XMC4100. All the CAN controllers I have worked in the past were quite s... Show More
User8683
XMC™
Hello,I am attempting to perform in circuit programming of my XMC1100 16 pin 64 KB flash MCU, but I am stuck because I cannot get MemTool to work prop... Show More
User11185
XMC™
I have an 8 bits gray encoder connected to the port P5.0 ...P5.7 of the XMC4500.Is there the possibility to get an interrupt every time a single pin c... Show More
User21901
XMC™
Hello 🙂I just have seen that the BCM5241XA1KMLG Ethernet transceiver used in the KIT_XMC48_RELAX_ECAT_V1 is discontinued.Is there any recommendation ... Show More
User18120
XMC™
Dear All,I would like to use an XMC4500 as a SPI master to talk to seven SPI slaves.Accordingly to the documentation, the XMC4500 has eight chip selec... Show More
User21483
XMC™
Hi,Please provide example code for XMC4800 Ethernet - TCP/IP & DHCP Protocol using XMCLib library without RTOS.Regards,Ashok Show More
User21649
XMC™
Reference Manual RTC, V3.2 - V1.3, 2016-08 page 11-16 and 11-17"Days counter starts with value 0 for the first day of month." incorrect, should be ... Show More
User21809
XMC™
Following the "XMC4300_Relax_EtherCat_APP_Slave_SSC-GS-v01_03-EN.pdf" I can't locate the example project referenced on pg.10. Where can that example b... Show More
User11520
XMC™
Hello everyone,I am trying to acquire a voltage with my XMC4500 Relax Kit and then transmit the value through USB.I am using the ADC_MEASUREMENT app a... Show More