Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

XMC™ Forum Discussions

chinhhd94
XMC™
Hello,I am fairly new to the XMC world and trying to communicate with mfrc522,  Could anyone please  pointout what 's wrong in my code, I try a lot bu... Show More
lila_young
XMC™
Hello, I add three TIMER APP in DAVE. One of them(TIMER_RxTimeout) has no problem during make. The other two has error: 'TIMER_BeforeTx' undeclared (f... Show More
NA97
XMC™
I have a custom board using the XMC4500F100X1024 microcontroller. Whenever I try to debug it using the link debugger, I receive the message 'No source... Show More
ziad-shaarawy
XMC™
I use Dave apps as SPI_Master to configure XMC1400 as the master in SPI communication, in the pin settings i configure the MOSI pin as Push-Pull then ... Show More
gargi1
XMC™
HRPWM Trap
solved msg Solved
Hi Team, i want to implement trap signal in hrpwm app. can anyone please share some setup steps or example code for referance. Thank, Gargi Show More
Rockeeee
XMC™
Peripheral Configuration * CCU80.CC80 - CC83 Configure as EA PWM,Frequency 20K,P0.12 Trap Event,Using MCM mode When no trap event occurs, everything i... Show More
Murali1
XMC™
Hi, I am using DAVE CE IDE , I faced one issue is  in XMC4108 controller .while debugging it is  not hitting the break points of Interrupts  . It is d... Show More
Mbaumgartner
XMC™
Hello, I'm currently trying to run a simple program on the XMC 1100 Boot Kit using Arduino IDE 2.3.2 following the steps highlighted in this guide: https://community.infineon.com/t5/Projects/XMC-For-Arduino/ba-p/436495... Show More
SunshineQAQ
XMC™
Hi, I use xmc-link can not give xmc7100 chip emulation, and after burning the program once, the program then burned in there is no reaction, why? Best... Show More
NA97
XMC™
I'm trying to display something on the serial terminal using UART. I got the example code and ran it on XMC4500 using DAVE IDE. However, I couldn't fi... Show More