XMC™ Forum Discussions
Hi,
We have this figure in the reference manual.
17.8.2 Data Alignment
How we have to interpret this in 12-bit mode? We have 16-bit result in 12-bit mode?
Show Less
Hi,
I'd like to increase the font size in the peripheral view. How to do that? I tried everything in Window/Preferences/Appearance but it doesn't help.
I have Dave 4.4.2
Show Less
using XMC1302 with PMSM_FOC App
the value of Motor_resistance and Motor_inductace are phase or phase-to-phase ?
Hi,
I'm new to the DAVE 4.5.0 IDE and have been trying to flash an EtherCat example project to the XMC4800 Automation Board V2, which builds successfully.
However, trying to debug the project with the board connected via USB gives the error "No emulators connected via USB". I do have the J-Link V634h driver installed, which is found by DAVE. Running the J-Link commander gives the same error message, and in device manager the board only shows up as "USB serial device(COM10)" and not as a J-Link device. The board is powered by 24v (I've included a photo to indicate the boards power status, the top right LED is flashing between red and green). Hopefully I've just overlooked something simple.
Is there anything else I can do so that the board is recognised as a J-Link device?
Many thanks,
Ben
Show Less
Hello team,
I have a problem while connecting XMC4400 hexagon to memtool 5. I followed the slide supported in the link below. But it can not connect to my PC. Is there anything I need to focus?
Thank you!
Show Less
Hello,
I have an XMC4800 Automation Board and I want to make it work from external ram. I saw the example project with ram test. But I want mcu to use external SDRAM automatically. So I suppose I should modify linker script but I don't know how to do it. Is there an example project with an already altered linker script?
Show LessHi,
Could somebody explain what does the gating input exactly in ADC? The trigger signal is clear for me.
Hello,
I would like to generate a binary program with DAVE 4 in order to calculate the CRC32 of my project.
what I do :
Then, I build project to generate .bin, but In folder Release I just have .lst and not .bin
How can I have this file ?
Already thank you,
Pierre Gachet
Show Less