- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hey,
I have problems to get the CAN FD demo running in a multicore project.
Code base is the CAN FD Demo --> in single Core Project everything works fine.
Open a Multicore Project --> Copy and Paste the code from the Example + design.modus file (tried the same manually-->same result)
The result on o Digital Analyzer after : "Cy_CANFD_UpdateAndTransmitMsgBuffer"
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
problem solved. --> missing P1_0 for CAN_STB. --> could you add this to the BSP defines? Same as all other pins?
this PIN is missing by default.
BR
Andreas
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I'm attaching a CAN FD + ADC project.
ADC is running on core 7_0 and CAN FD on core 7_1, there is an IPC channel that sends value from 7_0 to 7_1.
This is not an optimized/perfect project but an exercise, but it should hopefully help you anyway.
Import by clinking File-> Import -> General -> Existing Project into Workspace ...
You sometimes have to re-include the nested projects in the main project by right-clicking on them.
Be careful about the speed of CAN-FD which can be different from your need (change it in the Device configurator).
If you have any questions/problems, please right.
Best regards.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
problem solved. --> missing P1_0 for CAN_STB. --> could you add this to the BSP defines? Same as all other pins?
this PIN is missing by default.
BR
Andreas