Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

XMC™ Forum Discussions

Not applicable
Hi,

I am working on qSPI flash(S25FLO32P) available on-board using example code “SPI001_Example2 – qSPI mode”. The code is failing while setting the spansion flash to write enable “S25FL032P_WriteEnable”. I am not sure what could be the issue, below are my pin configurations. Anybody made it work?

p1.8 - CS Chipselect
p1.10 - CLK ClockOutput
p1.4 - DI - MRST/MTSR1HW
p1.5 - DO - MTSR0HW
p1.3 - WP - MTSR2HW
p1.2 - Hold - MTSR3HW
0 Likes
2 Replies
Not applicable
Hi,

According to the schematic, the DI should be connected to P1.5 and DO to P1.4.
Could this be the problem?

rgds,
Rou
0 Likes
Not applicable
Rou wrote:
Hi,

According to the schematic, the DI should be connected to P1.5 and DO to P1.4.
Could this be the problem?

rgds,
Rou

However I have tested and can confirm the following works.
p1.4 - DI - MRST/MTSR1HW
p1.5 - DO - MTSR0HW
0 Likes