Not applicable
Feb 27, 2015
08:10 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Feb 27, 2015
08:10 AM
Hi,
I'm using the XMC4500 and attempting to run the Dave3 example USBBL001_USBMS001.
- When plug in the USB drive, it doesn't create a dir/file
- I'm using XMC4500-1024-F144 AB
- I have updated all the Dave tools
- I've looked at the ERRATA and i don't believe the 2 issues listed are what I'm seeing.
- Ive tried rebuilding the example from the dave app SLTHA001
In Main, it does recognizes the drive and calls FATFS_TestDemo() when it plugs in.
- Once it tries to access the drive by f_mkdir OR f_open a USB interrupt occurs indefinitely and never returns to back to MAIN
- the USB drive light turns on, the VBUS_DRIVE works
- I've verified USB ID P0.9 is grounded to signal HOST Mode
GINTSTS_HOSTMODE is 0x600003b or 0x400003b at the start of every interrupt
- ModeMis = 1 (Mode Mismatch Interrupt is set, i think this is part of the main problem)
- Sof = 1
- RxFLvl = 1
- HChInt = 1 / 0
- PTxFEmp = 1
Have you seen this before? What can I try next?
Thanks
I'm using the XMC4500 and attempting to run the Dave3 example USBBL001_USBMS001.
- When plug in the USB drive, it doesn't create a dir/file
- I'm using XMC4500-1024-F144 AB
- I have updated all the Dave tools
- I've looked at the ERRATA and i don't believe the 2 issues listed are what I'm seeing.
- Ive tried rebuilding the example from the dave app SLTHA001
In Main, it does recognizes the drive and calls FATFS_TestDemo() when it plugs in.
- Once it tries to access the drive by f_mkdir OR f_open a USB interrupt occurs indefinitely and never returns to back to MAIN
- the USB drive light turns on, the VBUS_DRIVE works
- I've verified USB ID P0.9 is grounded to signal HOST Mode
GINTSTS_HOSTMODE is 0x600003b or 0x400003b at the start of every interrupt
- ModeMis = 1 (Mode Mismatch Interrupt is set, i think this is part of the main problem)
- Sof = 1
- RxFLvl = 1
- HChInt = 1 / 0
- PTxFEmp = 1
Have you seen this before? What can I try next?
Thanks
- Tags:
- IFX
0 Replies