Nov 04, 2013
09:54 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Nov 04, 2013
09:54 PM
The total power supply current defined below consists of a leakage and a switching component. Application relevant values are typically lower than those given in the following tables, and depend on the customer's system operating conditions (e.g. thermal connection or used application configurations).
If not stated otherwise, the operating conditions for the parameters in the following table are: VDDP = 3.3 V, TA = 25 deg C
If not stated otherwise, the operating conditions for the parameters in the following table are: VDDP = 3.3 V, TA = 25 deg C
0 Replies