Attachments are accessible only for community members.
Not applicable
Jun 21, 2016
12:24 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jun 21, 2016
12:24 AM
Hello,
I am using a XMC4500 with a physical chip from Micrel (KSZ8863mll).
I'd like to use the advanced functions like power saving features and cable diagnostics.
In order to do that, I need to send Messages with OPCODE=00b. See in the attached datasheet page 33
The XMC's reference manual only mentions OPCODES 10b and 01b (chapter 15.2.8.1).
Anybody knows a way to set the OPCODE directly?
Thanks, Michael
I am using a XMC4500 with a physical chip from Micrel (KSZ8863mll).
I'd like to use the advanced functions like power saving features and cable diagnostics.
In order to do that, I need to send Messages with OPCODE=00b. See in the attached datasheet page 33
The XMC's reference manual only mentions OPCODES 10b and 01b (chapter 15.2.8.1).
Anybody knows a way to set the OPCODE directly?
Thanks, Michael
- Tags:
- IFX
- xmc4500 eth
0 Replies