Jan 18, 2021
07:44 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jan 18, 2021
07:44 PM
No combination of TX/RX pins in the DAVE UART app within the DAVE IDE prints out to the Serial port when connected to my computer, I am using the below code to print numbers to UART:
Nothing will print to serial on baud rate 19200 with the following TX/RX combinations in the UART App in DAVE:
I build the .hex files in the DAVE IDE and then flash them to my boards with the XMC flasher app in the Infineon toolbox.
Is my board broken? Or is DAVE broken?
#include
#include
int main(void)
{
DAVE_STATUS_t status;
status = DAVE_Init(); /* Initialization of DAVE APPs */
if(status != DAVE_STATUS_SUCCESS)
{
XMC_DEBUG("DAVE APPs initialization failed\n");
}
while(1U)
{
int x = 0;
while (1U) {
char buffer[20];
sprintf(buffer, "%d \n", x);
x++;
UART_Transmit(&UART_0, buffer, strlen(buffer));
}
}
}
Nothing will print to serial on baud rate 19200 with the following TX/RX combinations in the UART App in DAVE:
- TX = P2.5, RX = P2.2
- TX = P0.1, RX = P0.0
- TX = P0.5, RX = P0.4
- TX = P1.5, RX = P1.4
I build the .hex files in the DAVE IDE and then flash them to my boards with the XMC flasher app in the Infineon toolbox.
Is my board broken? Or is DAVE broken?
Solved! Go to Solution.
1 Solution
Jan 19, 2021
06:14 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jan 19, 2021
06:14 AM
Hello,
How are the UART pins connected to the computer? Are you using the onboard breakable debugger of Distance2Go kit for UART communication?
Onboard debugger uses the pins UART TX = 0.1 and UART RX = 0.0 for UART communication. It is mentioned in page 33 of the application note.
Onboard debugger require SEGGER J-Link driver, make sure it is installed on your computer. Also, please double check that the UART settings are matching between the Distance2Go kit and the PC software.
Thanks and Regards,
Sudheesh
How are the UART pins connected to the computer? Are you using the onboard breakable debugger of Distance2Go kit for UART communication?
Onboard debugger uses the pins UART TX = 0.1 and UART RX = 0.0 for UART communication. It is mentioned in page 33 of the application note.
Onboard debugger require SEGGER J-Link driver, make sure it is installed on your computer. Also, please double check that the UART settings are matching between the Distance2Go kit and the PC software.
Thanks and Regards,
Sudheesh
1 Reply
Jan 19, 2021
06:14 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jan 19, 2021
06:14 AM
Hello,
How are the UART pins connected to the computer? Are you using the onboard breakable debugger of Distance2Go kit for UART communication?
Onboard debugger uses the pins UART TX = 0.1 and UART RX = 0.0 for UART communication. It is mentioned in page 33 of the application note.
Onboard debugger require SEGGER J-Link driver, make sure it is installed on your computer. Also, please double check that the UART settings are matching between the Distance2Go kit and the PC software.
Thanks and Regards,
Sudheesh
How are the UART pins connected to the computer? Are you using the onboard breakable debugger of Distance2Go kit for UART communication?
Onboard debugger uses the pins UART TX = 0.1 and UART RX = 0.0 for UART communication. It is mentioned in page 33 of the application note.
Onboard debugger require SEGGER J-Link driver, make sure it is installed on your computer. Also, please double check that the UART settings are matching between the Distance2Go kit and the PC software.
Thanks and Regards,
Sudheesh