Not applicable
Mar 07, 2016
04:17 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Mar 07, 2016
04:17 AM
Hello
The accuracy of the internal fast RC-oscillator in factory calibration is +-15% according to the datasheet.
Via the internal slow clock source (+-5%) and automatic calibration the reachable accuracy schould be +-5.5%.
Is there any possibility for further enhancement of the internal oscillator accuracy by additional trimming or anything similar?
Thanks
The accuracy of the internal fast RC-oscillator in factory calibration is +-15% according to the datasheet.
Via the internal slow clock source (+-5%) and automatic calibration the reachable accuracy schould be +-5.5%.
Is there any possibility for further enhancement of the internal oscillator accuracy by additional trimming or anything similar?
Thanks
Labels
- Tags:
- IFX
0 Replies