Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Travis
Employee
Employee
First solution authored Welcome! 500 replies posted
1701.attach

› Use a FIFO structure to store results in a safe way
› Some applications require extreme fast conversions. On the other hand, the CPU load (control loop for example) might load the CPU in a way that can limit how fast the results of the VADC conversions are read. In these cases, the VADC FIFO result structure will help to conserve results safely, avoiding overwriting, without having to force the CPU to read or slow down the converting rate.
› Up to a 16 stages FIFO can be built by means of concatenating result registers. Data reduction mechanisms (filtering, accumulation) as well as event generation is still valid and applicable.
0 Likes
0 Replies