XMC1400 - Maximum MCLK/PCLK frequency before going to deep sleep mode

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Not applicable
Hi,

Could anyone please help me to clarify which is the maximum frequency allowed in the MCLK/PCLK clock domain before entering deep sleep mode?
In the reference manual there is the following note, but I did not find any guidance, table or reference value.

XMC1400 AA-Step Microcontroller Series for Industrial Applications
Reference Manual V1.0 2015-10
Section: 14.3.2 System States
Subsection: Deep-Sleep State


Note: It is recommended to slow down the PCLK and MCLK before entering deep sleep mode to prevent a sudden load change that could cause a brownout reset.


My current setup:
XMC1404 running form main oscillator DCO1 = 48MHz = MCLK = PCLK
0 Likes
1 Reply