Not applicable
Mar 29, 2015
07:46 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Mar 29, 2015
07:46 AM
Hello,
I have issue with ports 2.10 and 2.11. IO004 app does not work. IO004_ReadPin() returns one and same value regardless of the level of that pin. I have tried it to combine them and use IO003 but without success. IO002 is not working too. I need to read those as a part from my device DMX address. Do I need to use anything additional?
Unfortunatelly I do not have time for debugging the HW or Infineon. I thought it will work as they say?!
Thanks
I have issue with ports 2.10 and 2.11. IO004 app does not work. IO004_ReadPin() returns one and same value regardless of the level of that pin. I have tried it to combine them and use IO003 but without success. IO002 is not working too. I need to read those as a part from my device DMX address. Do I need to use anything additional?
Unfortunatelly I do not have time for debugging the HW or Infineon. I thought it will work as they say?!
Thanks
- Tags:
- IFX
2 Replies
Not applicable
Mar 29, 2015
10:40 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Mar 29, 2015
10:40 PM
Hi,
Port 2 is an analog port, hence the pins need to be enabled as digital input in order to work.
For analog pin configuration, you need to use IO001 app instead of IO004.
Port 2 is an analog port, hence the pins need to be enabled as digital input in order to work.
For analog pin configuration, you need to use IO001 app instead of IO004.
Not applicable
Mar 31, 2015
05:20 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Mar 31, 2015
05:20 AM
Thanks. It works now!