Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

XMC™ Forum Discussions

User7109
Level 1
Level 1
Hello,

I want to use all 6 UARTs from the XMC4500 (F144 or E144 package). But if I try to add more than 4 UARTs to the Dave CE Project it is not possible. I get the message "HW resources not sharable constraint. Please check if the device has enough resources." The device should have 6 USICs, or? At the Moment the only Apps within the Project are the UART001 Apps. But it is the same result if I try to add SPI001 App.

All Updates for Dave/Apps were done.
What can I do to use all USICs?

Karsten
0 Likes
1 Reply
Not applicable
KaWi wrote:
Hello,

I want to use all 6 UARTs from the XMC4500 (F144 or E144 package). But if I try to add more than 4 UARTs to the Dave CE Project it is not possible. I get the message "HW resources not sharable constraint. Please check if the device has enough resources." The device should have 6 USICs, or? At the Moment the only Apps within the Project are the UART001 Apps. But it is the same result if I try to add SPI001 App.

All Updates for Dave/Apps were done.
What can I do to use all USICs?

Karsten


Hi Karsten,

This topic has been discuss previously.
Please do a search before ask.
http://www.infineonforums.com/threads/548-Incorrect-USIC-resources-handling-in-DAVE


rgds,
Rou
0 Likes