Why after Generate code, the changes I made in the linker_script.ld file were deleted?

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Yehudit
Level 1
Level 1
10 sign-ins 5 sign-ins First reply posted

Hello,

I use ABM in my code, so I have some additional code that I need to add to the linker_script.ld file.

My problem is that when I press the GENERATE code button (after changing or adding an App) the changes in the linker_script.ld file are deleted and it returns to the original.

why is it happening?

thanks 

Yehudit

0 Likes
1 Solution
LeoMathews
Moderator
Moderator
Moderator
First question asked 500 replies posted 100 solutions authored

Hi @Yehudit 

Can you please provide more information about the device you are using? Also, can you specify which IDE you are using? I believe you require to create a custom linker script and provide its path as a post-build command to use your desired linker script in the project.

Thanks and Regards,
Leo

View solution in original post

0 Likes
2 Replies
LeoMathews
Moderator
Moderator
Moderator
First question asked 500 replies posted 100 solutions authored

Hi @Yehudit 

Can you please provide more information about the device you are using? Also, can you specify which IDE you are using? I believe you require to create a custom linker script and provide its path as a post-build command to use your desired linker script in the project.

Thanks and Regards,
Leo

0 Likes
LeoMathews
Moderator
Moderator
Moderator
First question asked 500 replies posted 100 solutions authored

Hi @Yehudit  ,

Thread was locked due to inactivity for long time, you can continue the discussion on the topic by opening a new thread with reference to the locked one. The continuous discussion in an inactive thread may mostly be unattended by community users.

Thanks and Regards,
Leo

0 Likes