Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
Not applicable
Hi,
I have generated a project to obtain high sampling rate of VADC using XMC4500-F100x1024 Relax Lite Kit. But the output graph I generated seems like the sampling is not good enough..Can anybody tell me
what I did wrong in the VADC settings. I am hereby attaching my VADC settings as well as some screenshots of the output graph.

pics:-




VADC Settings:-



Thanks in advance...
0 Likes
3 Replies
User12775
Level 5
Level 5
First solution authored First like received
Which channel is which signal?

For example, what is the original signal shape?
0 Likes
Not applicable
Hi Aurixuser,
CH2 is actually what I am moitoring..Rightnow sine wave signal is connected to that channel..the frequencies i mentioned in the pictures are what i connected from a signal generator to the corresponding
VADC pin..Actually, if i connect the input from functionn generator to any four VADC channels that i am using will give me the same output graphs..From my observation what i can see is while using
four stage FIFO in VADC and if i enable result event after the 4th conversion , all the four result registers contains the same result even though the input signal frequency is too high.

Thanks in advance...
0 Likes
lock attach
Attachments are accessible only for community members.
User12775
Level 5
Level 5
First solution authored First like received
Please check if this example could help you.

0 Likes