Using XMC4700 firmware on CYBT-213043-EVAL

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Taylor70
Level 3
Level 3
First solution authored 10 replies posted 50 sign-ins

Hi there

I have a question about Modus Toolbox and my CYBT-213043-EVAL

My plan is to use an XMC4700 with an EPD display, but there were no XMC's available so I bought a CYBT-213043-EVAL

Would I be able to upload an XMC4700 BSP in Modus to my CYBT-213043-EVAL, and write the code to program the EPD display? I ask because both have the same core (PSoC 4)

Hope that makes sense

Cheers

0 Likes
1 Solution
LinglingG_46
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 10 questions asked

1: As my understanding, the XMC4700 and CYBT-2013043-EVAL are two different chips.  But if you want to modify the BSP, please refer to tips 2 and 3.  Please note that:

The best way to create a custom PSoC 6 BSP is to start with the BSP that closely matches your board requirements and customize it.

2: Please refer to the KBA:

https://community.infineon.com/t5/Knowledge-Base-Articles/Creating-Custom-BSPs-in-ModusToolbox-KBA23...

3: Please refer to the BSP assistant :

https://www.infineon.com/dgdl/Infineon-ModusToolbox_BSP_Assistant_1.0_User_Guide-UserManual-v01_00-E...

 

View solution in original post

0 Likes
1 Reply
LinglingG_46
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 10 questions asked

1: As my understanding, the XMC4700 and CYBT-2013043-EVAL are two different chips.  But if you want to modify the BSP, please refer to tips 2 and 3.  Please note that:

The best way to create a custom PSoC 6 BSP is to start with the BSP that closely matches your board requirements and customize it.

2: Please refer to the KBA:

https://community.infineon.com/t5/Knowledge-Base-Articles/Creating-Custom-BSPs-in-ModusToolbox-KBA23...

3: Please refer to the BSP assistant :

https://www.infineon.com/dgdl/Infineon-ModusToolbox_BSP_Assistant_1.0_User_Guide-UserManual-v01_00-E...

 

0 Likes