Not applicable
Nov 25, 2017
09:30 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Nov 25, 2017
09:30 AM
Hi,
I'm planning on using the CCU8 to control a Full Bridge DC/DC Converter.
I read in the XMC4500 reference manual, that you can do a phase shifted PWM by linking the timer cells.
How can I do that in DAVE?
Right now, I am using two PWM Apps in asynchronous mode where I set a 180° phase shift by
setting the starting point of the one at 0 and the other at 5000 and then start them simoultaneously.
Is this the way to go or is there a better way?
Because right now I need to use a function, that calculates the correct values, to set a dutycycle.
Thanks
I'm planning on using the CCU8 to control a Full Bridge DC/DC Converter.
I read in the XMC4500 reference manual, that you can do a phase shifted PWM by linking the timer cells.
How can I do that in DAVE?
Right now, I am using two PWM Apps in asynchronous mode where I set a 180° phase shift by
setting the starting point of the one at 0 and the other at 5000 and then start them simoultaneously.
Is this the way to go or is there a better way?
Because right now I need to use a function, that calculates the correct values, to set a dutycycle.
Thanks
- Tags:
- IFX
0 Replies