Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User15069
Level 1
Level 1
Hello

I tried to get the UART working on Pins P0.6 / P0.7 but with no success. Same code is working for USIC0.C0 on Pins P2.0 /P2.6.
I think, the hardware of the board but nothing happens on output pin P0.6.

According to the datasheet, the initialization steps should be ok, but it seems there is something missing...

Best regards and thank you for your hints

Geri



void InitUartC0C1(void)
{
#define UART_RX P0_7
#define UART_TX P0_6

/* UART configuration */
const XMC_UART_CH_CONFIG_t uart_config = {
.baudrate = 115200,
.data_bits = 8U,
.parity_mode = XMC_USIC_CH_PARITY_MODE_NONE,
.stop_bits = 1U
};

XMC_UART_CH_Init(XMC_UART0_CH1, &uart_config);
XMC_UART_CH_SetInputSource(XMC_UART0_CH1,
XMC_UART_CH_INPUT_RXD,USIC0_C1_DX1_P0_7);

/* Start UART channel */
XMC_UART_CH_Start(XMC_UART0_CH1);

/* GPIO configuration */
const XMC_GPIO_CONFIG_t rx_conf = {
.mode = XMC_GPIO_MODE_INPUT_TRISTATE,
.input_hysteresis = XMC_GPIO_INPUT_HYSTERESIS_STANDARD
};
const XMC_GPIO_CONFIG_t tx_conf = {
.mode = XMC_GPIO_MODE_OUTPUT_PUSH_PULL_ALT7,
.output_level = XMC_GPIO_OUTPUT_LEVEL_HIGH
};

/* Configure GPIO, */
XMC_GPIO_Init(UART_TX,&tx_conf); /* UART TX */
XMC_GPIO_Init(UART_RX,&rx_conf); /* UART RX */
}

void main(void)
{
InitUartC0C1();
while(1)
{
XMC_UART_CH_Transmit(XMC_UART0_CH1, 0x12);
}
}
0 Likes
2 Replies
jferreira
Employee
Employee
10 sign-ins 5 sign-ins First like received
Hi,

I cannot see anything wrong in your program.
Actually I tested with a XMC1100 Bootkit and it is working fine, i.e. activity is seen in the LED connected to P0.6.

Regards,
Jesus
0 Likes
User15069
Level 1
Level 1
Hello Jesus

Thank you for your feedback! I tested with my Oscilloscope on two boards. Really strange. Will perform some further tests.

Best regards and thanks again
Geri
0 Likes