Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

XMC™ Forum Discussions

User10969
Level 1
Level 1
Hello everyone,

I currently try to setup the SPI flash driver as master on XMC4500 for an external flash device.
Since output data (from flash device) is available from the falling edge of SCK, I am looking for the correct setting for the SPI interface on XMC,
sofar I didn´t find it. Could someone give me a hint about it ?

On Oscilloscope I could see that the read command sent to flash device, and output data from flash device, all are correct...only XMC4500 read it wrong.

If there is a SPI flash driver available as example for the XMC4500, I would be appreciated to know where I can find it.

Thanks in advance.
0 Likes
0 Replies