Attachments are accessible only for community members.
Nov 10, 2020
11:36 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Nov 10, 2020
11:36 PM
Hi,
I am trying to get the external Flash to work on the relax kit for the xmc4500 using the provided sample App SPI_EXAMPLE_XMC45.
I migrated the project to the XMC4500-F100x1024 architecture and modified the pin settings to the following:
Furthermore, in the App dependencies screen for SPI_MASTER_0, I used the following settings (in combination with all the different 4 clock settings):
Nonetheless, it seems that after a write-enable the returned status (see in the attached main.c:143) is 0 and not 2, therefore the operation fails.
I even had the provided flash chip on the relax kit card replaced with another flash chip from Cypress (S25FL128L) but I get identical results.
Any ideas what I am missing?
It would be great if a sample App was provided for the relax kit as well.
Thank you in advance.
I am trying to get the external Flash to work on the relax kit for the xmc4500 using the provided sample App SPI_EXAMPLE_XMC45.
I migrated the project to the XMC4500-F100x1024 architecture and modified the pin settings to the following:
Furthermore, in the App dependencies screen for SPI_MASTER_0, I used the following settings (in combination with all the different 4 clock settings):
Nonetheless, it seems that after a write-enable the returned status (see in the attached main.c:143) is 0 and not 2, therefore the operation fails.
I even had the provided flash chip on the relax kit card replaced with another flash chip from Cypress (S25FL128L) but I get identical results.
Any ideas what I am missing?
It would be great if a sample App was provided for the relax kit as well.
Thank you in advance.
- Tags:
- IFX
0 Replies