Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Not applicable
Hi all,

I want to transfer data from the microcontroller to the PC using RS232. I know that this is possible using USIC0, Channel 0 because of the Infineon driver, this also works. Unfortunately, I cannot use this Channel because it is already occupied... Now I use USIC1, Channel 1 for RS232 and I use a RS232-to-USB-level converter, but data on the PC are no longer correct!

Does anybody have a hint for me? Is it the level converter, which one could I use or are the settings wrong?

Regards,
Michael
0 Likes
1 Reply
Not applicable
Hi Michael,

RS232 on PC is using UART protocol.
All USIC channels can be configured to UART protocol.
Do you mind to give more details on your hardware setup and connection?
0 Likes