Not applicable
Jun 29, 2016
09:30 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jun 29, 2016
09:30 PM
Hi,
I downloaded THE example code (HTTPSERVER_RAW) from Infineon web (C:\DAVEv4\XMC_Peripheral_Library_v2.1.2\XMCLib\examples\XMC4500_series\ETH\HTTPSERVER_RAW)
and run it in the xmc4500 relax kit. By following the instructions in the readme file, I am able to use PC's browser to control the LED at the kit board.
This is done by changing the setting on the PC's network with the static IP address.
Further more I tried to change the intranet's router setting and enable the port forwarding. I hope to access the board from outside the intranet. So far I am not successful.
This test environment is based on DHCP: all the devices are connected to the router with the dynamic IP.
My questions are:
1. THE example code can connect to other device through the static IP address and the DHCP function may not be built in?
2. Is it possible to mix the static and dynamic IP for connection in between them?
One more thing, the example code is not utilized with the DMA?
Regards,
Ming
I downloaded THE example code (HTTPSERVER_RAW) from Infineon web (C:\DAVEv4\XMC_Peripheral_Library_v2.1.2\XMCLib\examples\XMC4500_series\ETH\HTTPSERVER_RAW)
and run it in the xmc4500 relax kit. By following the instructions in the readme file, I am able to use PC's browser to control the LED at the kit board.
This is done by changing the setting on the PC's network with the static IP address.
Further more I tried to change the intranet's router setting and enable the port forwarding. I hope to access the board from outside the intranet. So far I am not successful.
This test environment is based on DHCP: all the devices are connected to the router with the dynamic IP.
My questions are:
1. THE example code can connect to other device through the static IP address and the DHCP function may not be built in?
2. Is it possible to mix the static and dynamic IP for connection in between them?
One more thing, the example code is not utilized with the DMA?
Regards,
Ming
- Tags:
- IFX
- web server lwip
0 Replies