Pinouts of DAP MINIWIGGLER?

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User20918
Level 1
Level 1
First solution authored
Hi,

I'm trying to use the DAP_MINIWIGGLER with a 10-pin connector. After I connected it to my laptop, I tried to measure the voltage between pin 3&5 using a DMM and it was 0V, then measured the voltage between pin 3&1 and it was also 0V ... according to my understanding it should be 5V ! Also I didn't notice any LED on after I connected the miniwiggler to the USB ! ... is this normal, or I have a malfunctioning DAP miniwiggler?

Also, I'd appreciate if I can get the schematic of the "KIT_DAP_MINIWIGGLER_USB"

5052.attach

Thanks,
Nour
0 Likes
1 Solution
Vasanth
Moderator
Moderator
Moderator
250 sign-ins 500 solutions authored First question asked
0 Likes
1 Reply
Vasanth
Moderator
Moderator
Moderator
250 sign-ins 500 solutions authored First question asked

Hi Nour,

Kinldy refer the following document.

https://www.infineon.com/dgdl/AP2400314_DAP_Connector.pdf?fileId=db3a3043183a9555011888ea09bf671b

 

Best Regards,
Vasanth

0 Likes