Not applicable
Feb 05, 2016
07:18 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Feb 05, 2016
07:18 AM
Hi there,
I am pretty much through with the development of the first application which was done using DAVE and the XMC1100 for arduino evaluation board.
In the next step the controller should go onto its own board and be tested with other hardware.
Preferrably I would like to add a connector for Jlink, so that DAVE can still be used to download the program and for debugging if needed.
Is there any documentation available that tells which Pins to use and other requrements. From the manual it looks like either P0.14/P0.15 or P1.2/P1.3 must be used.
thanks for your advice.
I am pretty much through with the development of the first application which was done using DAVE and the XMC1100 for arduino evaluation board.
In the next step the controller should go onto its own board and be tested with other hardware.
Preferrably I would like to add a connector for Jlink, so that DAVE can still be used to download the program and for debugging if needed.
Is there any documentation available that tells which Pins to use and other requrements. From the manual it looks like either P0.14/P0.15 or P1.2/P1.3 must be used.
thanks for your advice.
- Tags:
- IFX
1 Reply
Feb 10, 2016
12:44 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Feb 10, 2016
12:44 AM
Hi,
you can refer to the board manual.
you can refer to the board manual.