Move from eval board to dedicated board

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Not applicable
Hi there,

I am pretty much through with the development of the first application which was done using DAVE and the XMC1100 for arduino evaluation board.
In the next step the controller should go onto its own board and be tested with other hardware.
Preferrably I would like to add a connector for Jlink, so that DAVE can still be used to download the program and for debugging if needed.

Is there any documentation available that tells which Pins to use and other requrements. From the manual it looks like either P0.14/P0.15 or P1.2/P1.3 must be used.

thanks for your advice.
0 Likes
1 Reply
Travis
Employee
Employee
First solution authored Welcome! 500 replies posted
Hi,

you can refer to the board manual.
0 Likes