Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
PrathameshJ
Level 1
Level 1
5 likes given 5 replies posted 25 sign-ins

Hello,

I am using XMC4400 Platform2Go evaluation board for project development.

I am facing same problem as per @gargi1 : https://community.infineon.com/t5/XMC/Micro-USB-debugger/m-p/454394#M12877

I gone through the steps mentioned here but still not able to debug the board. Still No probes connected via USB pop-up is coming.

image (1).png

 

 

 

 

 

1. I want to know why still this message is coming?

2. Is USB drivers correctly not installed from SEGGER JLINK?

3. Is my laptop further need USB access for connection?

Regards,

Prathamesh.

0 Likes
1 Solution
Pradeep_PN
Moderator
Moderator
Moderator
250 sign-ins 100 solutions authored 25 likes received

Hi @PrathameshJ ,

The answers to your questions are :

1)The serial device is not getting detected so it seeking an TCP/IP connection. That is because of the J-Link version you have installed so please delete the current V7.94 and install the older version which is lesser than V7.88.

2)We believe they are installed correctly.

3)Please elaborate the third question.

Hope this help and let me know if you have any further queries.

Best Regards
Pradeep.

View solution in original post

0 Likes
2 Replies
Pradeep_PN
Moderator
Moderator
Moderator
250 sign-ins 100 solutions authored 25 likes received

Hi @PrathameshJ ,

The answers to your questions are :

1)The serial device is not getting detected so it seeking an TCP/IP connection. That is because of the J-Link version you have installed so please delete the current V7.94 and install the older version which is lesser than V7.88.

2)We believe they are installed correctly.

3)Please elaborate the third question.

Hope this help and let me know if you have any further queries.

Best Regards
Pradeep.

0 Likes

Hi @Pradeep_PN ,

Thank you for providing solution.

It worked for me. I am now installed SEGGER JLINK V7.88

 

Thanks & Regards,

Prathamesh.

0 Likes