Mar 02, 2020
03:32 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Mar 02, 2020
03:32 AM
Hi,
I am currently trying to connect two XMC4700 relax kits through usb to transfer data from one to the other. The idea is to use the fast mode of usb which is usually faster than other ports. I am using an otg micro usb to micro usb cable.
My question is, does the XMC4700 support host mode and if yes, do I need to make hardware changes on the board(connecting pins) or it can be done only by software?
Thanks in advance.
Kostadin
I am currently trying to connect two XMC4700 relax kits through usb to transfer data from one to the other. The idea is to use the fast mode of usb which is usually faster than other ports. I am using an otg micro usb to micro usb cable.
My question is, does the XMC4700 support host mode and if yes, do I need to make hardware changes on the board(connecting pins) or it can be done only by software?
Thanks in advance.
Kostadin
0 Replies