Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

XMC™ Forum Discussions

User22765
Level 1
Level 1
First question asked
Hello,

I have bought 3 DAPMINIWIGGLERUSBTOBO1 and I've connected them via USB to an USB-HUB.
Doing so, I've realized that via InfineonMemtool 4.5 I'm able to connect only to one MiniWiggler.... is there a way to configure the tool in order to recognize the 3 different wigglers and to switch to the one I want to select?
Attached the configuration I have on my laptop.
Thanks for support.
0 Likes
1 Solution
Vasanth
Moderator
Moderator
Moderator
250 sign-ins 500 solutions authored First question asked

Hi,

The tool has an option Use IO Pod .This selection is available when using communication devices where  multiple JTAG interfaces are available (e.g. UAD3). Select the target port you want. If (default) is selected, then the first available port is used. 

Best Regards,
Vasanth

View solution in original post

0 Likes
1 Reply
Vasanth
Moderator
Moderator
Moderator
250 sign-ins 500 solutions authored First question asked

Hi,

The tool has an option Use IO Pod .This selection is available when using communication devices where  multiple JTAG interfaces are available (e.g. UAD3). Select the target port you want. If (default) is selected, then the first available port is used. 

Best Regards,
Vasanth

0 Likes