Not applicable
Feb 01, 2018
07:31 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Feb 01, 2018
07:31 PM
Hi all,
I am now using Dave 4.2.3 with 64Bit and Distance2Go development board based on the XMC4200. I try to use sample code from "Dave Help --> USBD_VCOM" to enable the USB port and send the data out from USB.
For the current project, I've created the "USBD_VCOM" APP.
However, I meet the problem. When I execute the sample code step by step, and then enter into "while(!USBD_VCOM_IsEnumDone()); , it goes under the infinite loop condition and no longer can not trace the code..
On the other hand, when I connect the debug port to PC and also connect main port to the same/other PC, only debug port can be recognized. I am not sure if PC could recognize two ports from development board at the same time.
Can anybody share some advices that where the problem is or what have I to do to over USB to get the basic functionality??
Thanks for you helps,
Paul
I am now using Dave 4.2.3 with 64Bit and Distance2Go development board based on the XMC4200. I try to use sample code from "Dave Help --> USBD_VCOM" to enable the USB port and send the data out from USB.
For the current project, I've created the "USBD_VCOM" APP.
However, I meet the problem. When I execute the sample code step by step, and then enter into "while(!USBD_VCOM_IsEnumDone()); , it goes under the infinite loop condition and no longer can not trace the code..
On the other hand, when I connect the debug port to PC and also connect main port to the same/other PC, only debug port can be recognized. I am not sure if PC could recognize two ports from development board at the same time.
Can anybody share some advices that where the problem is or what have I to do to over USB to get the basic functionality??
Thanks for you helps,
Paul
- Tags:
- IFX
0 Replies